i.MX6 Solo Lite boot from eMMC fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Solo Lite boot from eMMC fail

521 次查看
m_c
Senior Contributor I

Customer found boot from eMMC fail and has two diagrams for boot okay and fail as below. In this design, only XTAL 24MHz is used and no RTC_XTAL. Is this fail because of ERR007927?

boot_success

boot_success.png

boot fail

boot_failure.png

标签 (1)
标记 (1)
0 项奖励
1 回复

360 次查看
art
NXP Employee
NXP Employee

Yes, the effect of the ERR007927 erratum is the likely cause of the issue.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励