i.MX6 SabreSD board stuck at boot animation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SabreSD board stuck at boot animation

Jump to solution
2,192 Views
zhencongtee
Contributor III

Greetings,

I am trying to do some development on the i.MX6 SabreSD (quad core) board from Freescale. I had successfully build the source following the Android User Guide.pdf document. However when i try to download the img that I build into the board using Mfgtool2.0, my image stuck at the boot animation with "android" logo at the middle of the display. I believe it's the android system.img that has problem, because if i use the u-boot-6q.bin, boot.img, recovery.img that i build with original system.img downloaded from Freescale website, it does not have the stuckissue.

Attach is the bootlog with the output from 'top' command to show the list of running processes.

Anyone please help? I am totally stucked at this stage and I have no idea how to proceed...

Thanks in advance for any kind help.

Regards,

ZC Tee

Labels (3)
0 Kudos
Reply
1 Solution
1,479 Views
zhencongtee
Contributor III

This problem is solved by using the latest BSP jb4.2.2_1.1.0 version.

View solution in original post

0 Kudos
Reply
5 Replies
1,480 Views
zhencongtee
Contributor III

This problem is solved by using the latest BSP jb4.2.2_1.1.0 version.

0 Kudos
Reply
1,479 Views
brajeshsharma
Contributor II

Hi Zhen ,

Can you please share the working init.rc , boot-log , logcat files or

whichever possible since that may help me .

0 Kudos
Reply
1,479 Views
zhencongtee
Contributor III
0 Kudos
Reply
1,479 Views
brajeshsharma
Contributor II

Hi Zhen ,

I am using the exact Android Version but still stuck with Android Start up

logo .

On Wed, Dec 4, 2013 at 6:56 AM, Zhen Cong Tee <admin@community.freescale.com

0 Kudos
Reply
1,479 Views
brajeshsharma
Contributor II

from where u have downloaded system.img which is working with ur build uboot and boot.img and recovery.img

which link =?

0 Kudos
Reply