i.MX6 Sabre SDP video does not always start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Sabre SDP video does not always start

Jump to solution
1,057 Views
wayne_s
Contributor II

I am running the 13.04.24 version of ltib (Linux version 3.0.35-2508-g54750ff), and video usually starts up during boot (I get 4 penguins while the kernel is booting, and the matchbox desktop comes up). 


Every now and then, I get no display on the LCD but the system seems to run fine otherwise.  Unblanking the display with:

    echo 0 >/sys/class/graphics/fb0/blank

    cat /etc/splash.bmp >/dev/fb0

    echo -e -n "\33[9;0]\33[14;0]" >/dev/console

 

does not do anything, so I don't believe it to be in the screen blanking subsystem.

 

Does anyone have suggestions on how to debug this problem?  It is an intermittent problem that happens with either resets or power cycling.  There are no differences in the dmesg output between a successful reboot with graphics and one without.

.

Thanks,

Wayne

Original Attachment has been moved to: boot_no_display.txt.zip

Labels (2)
Tags (2)
1 Solution
709 Views
wayne_s
Contributor II

This hasn't happened again since I switched to Yocto BSP and included 'ldb=dul0' on the kernel boot parameters line.

View solution in original post

2 Replies
709 Views
FranciscoCarril
Contributor V

Your issue is very hard to reproduce.

Have you tried with a different screen (hdmi for example) 

is it the same behavior?

0 Kudos
710 Views
wayne_s
Contributor II

This hasn't happened again since I switched to Yocto BSP and included 'ldb=dul0' on the kernel boot parameters line.