How to determine the value of (ResRef) RTerm calibration resistor on the SATA PHY?
On the "iMX6 Smart device system" the value is 191R 1%, why?
解決済! 解決策の投稿を見る。
Hi,
The closest I have come to a description of the resistor value, is found here:
Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors.
IMX6DQ6SDLHDG, Rev 1, 06/2013
Section 2.2 table 2-13
"SATA_REXT – Connect an external 191 Ω 1% resistor to GND."
"The impedance calibration process requires connection of this reference resistor.
If SATA is unused, the reference resistor may be populated if desired for manufacturability purposes, or left no-connect for cost savings."
/Martin.
Hi,
The closest I have come to a description of the resistor value, is found here:
Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors.
IMX6DQ6SDLHDG, Rev 1, 06/2013
Section 2.2 table 2-13
"SATA_REXT – Connect an external 191 Ω 1% resistor to GND."
"The impedance calibration process requires connection of this reference resistor.
If SATA is unused, the reference resistor may be populated if desired for manufacturability purposes, or left no-connect for cost savings."
/Martin.
Hi Martin
from MX6DQ sect.54.1.4 Block Descriptions :
"RTerm Tuning -This block uses an external resistor (ResRef) as reference to
determine the proper calibration setting for centering the Rx and Tx termination
resistances at 50 ohms."
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Chip,
Yes this is correct, I also found this description in the Reference manual.
But nothing about what the value of the resistor should be... That is my question..
Hi Martin
value you can find in i.MX6 SDP/SDB schematic
"MX6_SABRE_SDP_DESIGNFILES "
Best regards
chip