i.MX6 Quad 4GB DDR stress test issue (USB Device Not Recognized)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Quad 4GB DDR stress test issue (USB Device Not Recognized)

799 Views
m_c
Senior Contributor I

We use i.MX6 DDR Stress Test Tool V1.0.3 to test i.MX6 Quad with DDR3 4G. When start read/write delay calibration, the Windows PC shows USB Device Not Recognized). What should we check or fix for this issue?


pastedImage_1.png

Labels (1)
Tags (2)
0 Kudos
1 Reply

428 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

you can try other computer (preferably with Windows XP) also try through usb hub.

Additionally suggested to check if board USB interface works properly with SDK usb tests.

i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------