i.MX6 PWM Polarity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 PWM Polarity

1,567件の閲覧回数
ryanerb
Contributor III

I know the DIO on the i.MX6 supports PWM.


The question is, does it support changing the polarity of the PWM?

I attempted to set the polarity and it would not let me ....

root@imx6:~# echo inversed > /sys/class/pwm/pwmchip0/pwm0/polarity

-sh: echo: write error: Function not implemented

From the Linux pages online, it says:

polarity - Changes the polarity of the PWM signal (read/write). Writes to this property only work if the PWM chip supports changing the polarity. The polarity can only be changed if the PWM is not enabled. Value is the string "normal" or "inversed".

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,177件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ryan

according to description in Chapter 51 Pulse Width Modulation (PWM)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

polarity can not be changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,177件の閲覧回数
ryanerb
Contributor III

Hello Igor,

Chapter 51 states on page 4482:

• Active high or active low configured output

I would assume this indicates it does allow for polarity to be changed.

Please clarify and provide a copy/paste from the RM with a page number if possible.

Thank you,
Ryan

0 件の賞賛
返信

1,177件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ryan

it can be configured with PWMx_PWMCR[POUTC], p.4490,

sorry for overlooking.

Best regards

igor

0 件の賞賛
返信