i.MX6 MAX die temperature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 MAX die temperature

ソリューションへジャンプ
1,828件の閲覧回数
diegoferraiuolo
Contributor I

Hi,

in my application I'm using  an i.MX6-quad.

I measure the die temperature by:

cat/sys/class/thermal/thermal_zone0/temp.

What is the upper limit I should consider for this value  so that the product

works in a safe condition?

Thanks in advance.

Best Regards,

Diego

ラベル(1)
0 件の賞賛
返信
1 解決策
1,100件の閲覧回数
art
NXP Employee
NXP Employee

The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,100件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

The datasheet is located here:

http://www.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

you can check table 4.1.3

0 件の賞賛
返信
1,101件の閲覧回数
art
NXP Employee
NXP Employee

The maximum die temperature is sepcified as the 'Junction Temperature' parameter in the corresponding part's Data Sheet document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信