i.MX6 HAB support in U-Boot 2013 and later

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 HAB support in U-Boot 2013 and later

1,261件の閲覧回数
igorbezukh
Contributor I

Hi,

I would like to know whether HAB is supported in U-Boot 2013 or later versions?

Thanks and BR!

Igor Bezukh

ラベル(8)
0 件の賞賛
返信
1 返信

778件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Igor

yes supported, next Frescale linux kernel 3.10.17 Yocto release has U-boot 2013.4.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信