Hi,
I'm working on the implementation of a camera Omnivision 5653.
Is it possible ? If only the interface (DVP) is the same on board and on camera it will work ?
Can I use the camera under Android ?
Actually I've got an Omnivision 5653 and it works perfectly under Android.
Thanks for your help,
Armand
I can't find the folder for this :
Select specific camera drivers in the following location (as shown in figure below):
Device Drivers > Multimedia support > Video capture adapters > MXC Camera/V4L2 PRP Features support