i.MX6 DualLite + OV5653

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 DualLite + OV5653

3,992 Views
armandvignat
Contributor II

Hi,

I'm working on the implementation of a camera Omnivision 5653.

Is it possible ? If only the interface (DVP) is the same on board and on camera it will work ?

Can I use the camera under Android ?

Actually I've got an Omnivision 5653 and it works perfectly under Android.

Thanks for your help,

Armand

Labels (2)
8 Replies

1,555 Views
armandvignat
Contributor II

I'm sorry but I can go here : Device Drivers > Multimedia support > Video capture adapters

But I can't find  MXC Camera/V4L2 PRP Features support :s

0 Kudos

1,555 Views
jimmychan
NXP TechSupport
NXP TechSupport
  1. Attached is the BSP porting guide for Linux. You can take it as reference about porting the camera.
  2. For the Android BSP, we have a newer version available on the web. please use the latest version android_jb4.2.2_1.0.0. And I attached the FAQ of Android BSP. Please read the section 18 & 19 about the camera settings in android.

1,555 Views
alandeng
Contributor I

is it possible to paste the mentioned file:

ipuv3_csi0_chess.c

Thanks

0 Kudos

1,555 Views
armandvignat
Contributor II

I can't find the folder for this  :

Select specific camera drivers in the following location (as shown in figure below):

Device Drivers > Multimedia support > Video capture adapters > MXC Camera/V4L2 PRP Features support
Can you help me ?

0 Kudos

1,555 Views
jimmychan
NXP TechSupport
NXP TechSupport

it is not a folder. It is kernel configuration.

0 Kudos

1,555 Views
armandvignat
Contributor II

How do I get it ? The user guide doesn't explain how to do :s

0 Kudos

1,555 Views
jimmychan
NXP TechSupport
NXP TechSupport

go to the linux kernel , then type 'make menuconfig'.

1,555 Views
armandvignat
Contributor II

Nobody ? :s

0 Kudos