Hi
According to p7 of AN4467: https://www.nxp.com/docs/en/application-note/AN4467.pdf
ZQ calibration auto initialization mode is strongly recommended for keeping the ZQ registers calibrated during i.MX 6 Series operating modes and ambient temperature changes.
I guess some drivers in kernel done "force initiated hardware ZQ calibration" when temperature changed.
BTW I believe "auto initiated hardware ZQ calibration" done periodically.
Is my guess correct? (Is such recommendation supported by OS?)
Could someone let me know the url of the source code regarding above feature?
e.g https://source.codeaurora.org/external/imx/linux-imx/tree/drivers?h=imx_4.14.98_2.0.0_ga
已解决! 转到解答。
Hi torus
yes software performs calibartion in linux/arch/arm/mach-imx/ddr3_freq_imx6.S
in cpufreq driver described in attached Linux Manual when changing frequency
(also due to temperature)
ddr3_freq_imx6.S\mach-imx\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi torus
yes software performs calibartion in linux/arch/arm/mach-imx/ddr3_freq_imx6.S
in cpufreq driver described in attached Linux Manual when changing frequency
(also due to temperature)
ddr3_freq_imx6.S\mach-imx\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------