i.MX6 Android couldn't see my WMV files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Android couldn't see my WMV files

ソリューションへジャンプ
1,738件の閲覧回数
torus1000
Contributor V

Hi guys.

I just start to see Android4.3.1.1.0 demo with i.MX6DL-SDP but I couldn't find my *.mwv files in my Gallary.

My wmv can play without error on my PC and include WVC1 video(720P/1080P) and WMAP audio.

Does Android mediaserver support wmv files?

So I installed MX Player 1.7.26 and it could play them but some frames dropped.

This player had software decoder and I couldn't change to hardware(VPU).

Does i.MX6 VPU support VC-1 decode?

How can I play wmv file with VPU?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,239件の閲覧回数
torus1000
Contributor V

Sorry!

I found the release note which described special codec was need for WMV play.

Android_Codec_Release_Notes.pdf

? All video codecs are accelerated with the Video Processing Unit (VPU) except the

WMV7/8 decoder and the Sorenson H.263 decoder.

? All audio codecs are optimized by Freescale.

? WebM is enhanced by Freescale codecs.

? ASF, WMV, WMA, and AACPLUS need special codec package to be installed. <== Here !!

? MJPEG subtypes and MJPEG_2000 and MJPEG_B are not supported.

? MJPEG only supports YUV420 and YUV422 (horizontal) color formats.

? H.264 TS streams do not support seek and are only tested with limited streams.

https://community.freescale.com/thread/302737

Please apply to local Freescale FAE.

Windows Media Components Final Product Licensee should be approved prior to distribution.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,239件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Yes,  Android 4.3 does support VC-1.

Please take a look at the i.MX Android Codec Release Notes

1,239件の閲覧回数
torus1000
Contributor V

Dear SerchMX,

Thank you for the Release Notes and quick reply.

>Yes,  Android 4.3 does support VC-1.

I hope so but browser(video player) always said "Can't play this video".
If you have same board and demo, could you check sample wmv videos?
http://download.wavetlan.com/SVV/Media/HTTP/http-wmv.htm

Browser didn't play my local wmv neither, in spite of MX player could play w/ sw codec.
file:///udisk/my_local.wmv

Again, please let me know...
Does someone knows how to enable VPU for playing wmv videos?

0 件の賞賛
返信
1,240件の閲覧回数
torus1000
Contributor V

Sorry!

I found the release note which described special codec was need for WMV play.

Android_Codec_Release_Notes.pdf

? All video codecs are accelerated with the Video Processing Unit (VPU) except the

WMV7/8 decoder and the Sorenson H.263 decoder.

? All audio codecs are optimized by Freescale.

? WebM is enhanced by Freescale codecs.

? ASF, WMV, WMA, and AACPLUS need special codec package to be installed. <== Here !!

? MJPEG subtypes and MJPEG_2000 and MJPEG_B are not supported.

? MJPEG only supports YUV420 and YUV422 (horizontal) color formats.

? H.264 TS streams do not support seek and are only tested with limited streams.

https://community.freescale.com/thread/302737

Please apply to local Freescale FAE.

Windows Media Components Final Product Licensee should be approved prior to distribution.

0 件の賞賛
返信