i.MX53 Third USB host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Third USB host

620 Views
ToxicAvenger
Contributor III

Hello,

I have custom board based on i.MX53 with MC34708 PMIC.

I know that this board have 3 usb ports, but only two of them are used (one host and one OTG).

How to enable third USB?

Best regards.

Labels (3)
0 Kudos
Reply
1 Reply

530 Views
b36401
NXP Employee
NXP Employee

Please note that the Lower USB Host jack and the Micro USB Device jack

are cross connected. You can plug one cable into either jack,

but cannot plug cables into both jacks at the same time.

I can suggest to use some external USB hub to attach more USB devices.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply