i.MX53 Quick Start Board Hands-On training

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Quick Start Board Hands-On training

2,116 Views
rlorriaux
Contributor I

This is the Hands-On, i.MX53 Quick Start Linux/Android Training from Adeneo Embedded.

Labels (1)
0 Kudos
Reply
3 Replies

1,055 Views
LuisRivera
Contributor II

Hi, How can I do to request a class in Mexico city? because the link http://www.freescale.com/webapp/sps/site/training_information.jsp?c... its broken.

I'm interested on a one-day workshop.

Best regards,

Luis Rivera

0 Kudos
Reply

1,055 Views
JesseDannenbrin
Contributor I

You can get the flashing scripts from our latest release(3.3) of Android for the QS board available at: 

http://www.adeneo-embedded.com/en/Products/Board-Support-Packages/Freescale-i.MX53-QSB

 

Just click the download link and register for free. Once you've registered and signed in you can hit the download button again to receive FTP access to the Android BSP.

 

You should find the script in the 'scripts' folder once you've unpacked the i.MX53-QSB-Android-Release3.3.tar.gz file. A limitation of the flashing script is that it doesn't use the entire SD partition and requires a micro SD card that is >=2GB.

 

Note that there is 1 script for flashing the prebuilt binaries, and 1 for flashing binaries built from source using the provided scripts for building the QS board. This info is also available in the release notes which will be available to you once you have FTP access.


Jim Donelson said:

Thanks.
Are the flashing scripts mentioned on page 110 available for download?
I would like to try out Android on my QS board and it would be helpful.
0 Kudos
Reply

1,055 Views
JimDonelson
Contributor I
Thanks. Are the flashing scripts mentioned on page 110 available for download? I would like to try out Android on my QS board and it would be helpful.
0 Kudos
Reply