i.MX53 Linux screen rotate 180 degree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 Linux screen rotate 180 degree

1,174 Views
m_c
Senior Contributor I

We use L2.6.35_MX53_1109_PATCH_IMAGE on i.MX53 QSB. We can't rotate screen 180 degree by below command. Is there any other way can do this?

echo 3 > /sys/class/graphics/fb0/rotate

Labels (3)
0 Kudos
4 Replies

620 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi m.c

Was it useful the Community thread mentioned by Saurabh? Did you was able to rotate the screen?

Best regards!

/Carlos

0 Kudos

620 Views
m_c
Senior Contributor I

It can rotate 180 degree by user land program from Saurabh suggestion. However, customer needs rotate display in the begining when boot. If screen frame buffer can rotate in operating system level, the graphic application doesn't need modify anything. Can i.MX53 Linux support display rotate 180 degree in OS level?

0 Kudos

620 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi m.c

It seems that in the following thread they are also asking about rotate the screen during boot time, so you could try these implementations:

https://community.freescale.com/message/304789


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

620 Views
saurabh206
Senior Contributor III
0 Kudos