Hello,
I am working with i.MX535 QSB from Freescale in IAR EWARM. I had used GettingStarted example from IAR EWARM, modifying the project like shown below (main.c).
I am not able to get interrupts in IRQ_Handler address (0x18), even enabling TZIC #39. Anyone could please help me to get my LED on P7_7 blinking?
The code is working well when pooling GPTSR_bit.OF1 bit in while(1), like suggested in the original GettingStarted project. But I need to get interrupts directly from the interrupt vector, what I can easily do on ARM7 platform for example.
Thanks,
Tiago
/** include files **/
#include <Freescale/iomcimx535.h>
#include <intrinsics.h>
#include "board.h"
/* GPT1 Tick per second*/
#define GPT_TICK_PER_SEC 4
/** private data **/
static volatile Int8U Gpt1Counter;
volatile unsigned char flag0;
/**
*
*/
__irq void IRQ_Handler(void)
{
__DSB();
if (flag0 < 0xFF)
{
flag0++;
}
GPTSR_bit.OF1= 1;
__DSB();
return;
}
/**
*
*/
int main(void)
{
// USER LED init - GPIO_7[7]
IOMUXC_SW_MUX_CTL_PAD_PATA_DA_1_bit.MUX_MODE = 1;
GPIO7_DR_bit.no7 = 0;
GPIO7_GDIR_bit.no7 = 1;
// Init GPT
Gpt1Counter = 0;
// Select CKIL for timer clock - Low Frequency Reference Clock
GPTCR_bit.CLKSRC = 4;
// Init the Timer prescaler
GPTPR_bit.PRESCALER = 0;
// Init timer tick interval
GPTOCR1 = CKIL/GPT_TICK_PER_SEC;
//Enable Interrup on compare
GPTIR_bit.OF1IE = 1;
// Enable GPT1
GPTCR_bit.EN = 1;
/* Configure TZIC Interrupt Controller */
TZIC_ENSET1_bit.INTENSET39 = 1;
TZIC_INTSEC1_bit.SECURE39 = 1;
TZIC_PRIOMASK_bit.MASK = 0x1F;
TZIC_PRIORITY9_bit.PRIO39 = 0x20;
TZIC_INTCTRL = 0x80010001;
__enable_interrupt();
while (1)
{
if (flag0)
{
flag0 = 0;
++Gpt1Counter;
GPIO7_DR_bit.no7 = (1 & Gpt1Counter);
}
}
}