i.MX50: Where is the fuse for Muxed(low half) NOR Flash boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX50: Where is the fuse for Muxed(low half) NOR Flash boot

ソリューションへジャンプ
827件の閲覧回数
norishinozaki
Contributor V

Hello Champs,

I need to boot by NOR Flash in muxed at low half bits.

I understand I need to set 00 at BOOT_CFG2[7:6] in OCOTP.

However which addresses are these bits or fuse located?

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
1 解決策
728件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, You may also look at Table 23-1 (EIM multiplexing) of the i.MX50 Reference Manual.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
728件の閲覧回数
Yuri
NXP Employee
NXP Employee

BOOT_CFG2[7:6] corresponds OCOTP_CFG3[23:22] .

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
728件の閲覧回数
norishinozaki
Contributor V

Yuri,

Thanks,

So I set 00 in OCOTP_CFG3[23:22] for muxed 16-bit NOR Flash boot, the data and address pins are connected to the pads in Yellow?

pastedImage_0.png

Best regards,

Nori Shinozaki

0 件の賞賛
729件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, You may also look at Table 23-1 (EIM multiplexing) of the i.MX50 Reference Manual.

Regards,

Yuri.

0 件の賞賛
728件の閲覧回数
norishinozaki
Contributor V

Yuri,

Thank you!

I created a new thread for this question on a different subject, but please ignore it.

Best regards,

Nori Shinozaki

0 件の賞賛