Hi,
I used IMX_MFG_TOOL to program nand flash for i.MX28.
Connected - i.MX28 EVK Board Connected using USB-OTG to PC. PC detected it as HID complaint Device and i am successfully able to
update the nand flash using IMX_MFG_TOOL. Now, when i connect my customized i.MX28 hardware Board (similar to EVK Board), PC detects it as
Unknown device though i use same device driver supplied in IMX_MFG_TOOL software.
I followed these steps (on customized hardware),
Result - PC detects my customized board as Unknown device.
my question is am i missing any step or configuration, which is there in EVK Board and not on my customized Board, Or is it something else?
Any help would be appreciated, Thanks in advance.
解決済! 解決策の投稿を見る。
It might work, but I’m not sure as I never tried it like that. I think zImage for “Manufacturing Firmware” profile also has some options enabled that are required for proper operation and it could be much bigger than what is really needed. So probably makes sense to do have a separate LTIB setup for updater firmware binary.
Thanks Vladan, Just a quick clarification.
We had a ltib setup through which we used to generate imx28_ivt_linux.sb and flash it to SD card and bring up the board.
Now for MFG tool, We modified the same LTIB setup to manufacturing firmware profile and generated updater_ivt.sb.
We would like to know whether updater_ivt.sb shall work for mfgtool. or
do we have to install new ltib setup with manufacturing firmware profile selected at beginning.
or
should we copy all the binaries (power_prep, boot_prep, linux_prep, zlmage and initramfs image) to separate folder and run the script create_updater.sh from the folder. These binaries are created from ltib setup that has "manufacturing firmware profile" .. is there any chance it would work.
It might work, but I’m not sure as I never tried it like that. I think zImage for “Manufacturing Firmware” profile also has some options enabled that are required for proper operation and it could be much bigger than what is really needed. So probably makes sense to do have a separate LTIB setup for updater firmware binary.
Thank you Vladan, now i am able to flash NAND in my Board.
Please notice the kernel panic in the end .
Please follow this link to see the log file of debug prints for custom board and 1GB NAND https://skydrive.live.com/redir?resid=31ADA173C8B155A8!111&authkey=!AF7gOtgyU9ZNa84
and also there is log for EVK (i.MX28) with 1GB NAND on borad, which is : Microsoft SkyDrive - Access files anywhere. Create docs with free Office Web Apps.
... I can see kernel config diff between EVK and My kernel but still i am missing something. . any idea?
I don't see an option here to attach any file other than image. i'll find out a way to send you the log, anyway. Thanks
^^*Correction I am sorry MT29F1G08ABADAWP is 1GB. I have 1GB NAND on my customized board.