Hi
Im trying to build a linux image for i.mx28EVM utilizing the latest LTIB L2.6.35_1.1.0_130130
The build fails with ipsec-tools package
Here is the output from LTIB
Processing: ipsec-tools
=========================
Build path taken because: directory build, build key set, no prebuilt rpm,
rpmbuild --dbpath /home/icheifot/WORK/Freescale/i.MX28/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/icheifot/WORK/Freescale/i.MX28/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/icheifot/WORK/Freescale/i.MX28/ltib/tmp' --define '_rpmdir /home/icheifot/WORK/Freescale/i.MX28/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/icheifot/WORK/Freescale/i.MX28/ltib/dist/lfs-5.1/ipsec-tools/ipsec-tools.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/icheifot/WORK/Freescale/i.MX28/ltib/tmp/rpm-tmp.46463
+ umask 022
+ cd /home/icheifot/WORK/Freescale/i.MX28/ltib/rpm/BUILD
+ cd ipsec-tools-0.7.1
++ echo arm-none-linux-gnueabi-
++ sed -e 's,-$,,'
+ export X_DIR=arm-none-linux-gnueabi
+ X_DIR=arm-none-linux-gnueabi
++ perl -p -e s,/bin/arm-none-linux-gnueabi-gcc,,
++ which arm-none-linux-gnueabi-gcc
+ export TC_PREFIX=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi
+ TC_PREFIX=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi
+ echo /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi
/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi
++ perl -e '
foreach $path ("$ENV{TC_PREFIX}/$ENV{X_DIR}/include/linux/version.h",
"$ENV{TC_PREFIX}/include/linux/version.h",
"$ENV{TC_PREFIX}/arm-fsl-linux-gnueabi/multi-libs/default/usr/include/linux/version.h",
"$ENV{TC_PREFIX}/$ENV{X_DIR}/sysroot/usr/include/linux/version.h",
"$ENV{TC_PREFIX}/$ENV{X_DIR}/libc/usr/include/linux/version.h") {
if(-f $path) {
warn "found $path";
$path = @ARGV = ($path);
last;
}
}
warn("Cannot find version.h\n"), exit(1) unless @ARGV;
$path = $ARGV[0];
while(<>) {
m,UTS_RELEASE\s+"2\.(\d), && do { $lin_series = $1; last };
}
if($lin_series eq "4") {
print "$ENV{DEV_IMAGE}/usr/src/linux/include";
} else {
$path =~ s,/linux/version.h,,;
print $path;
}
exit(0);
'
Cannot find version.h
+ KHDR=
error: Bad exit status from /home/icheifot/WORK/Freescale/i.MX28/ltib/tmp/rpm-tmp.46463 (%build)
RPM build errors:
Bad exit status from /home/icheifot/WORK/Freescale/i.MX28/ltib/tmp/rpm-tmp.46463 (%build)
Build time for ipsec-tools: 0 seconds
Failed building ipsec-tools
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Mon Feb 25 17:02:49 2013
Ended: Mon Feb 25 17:02:50 2013
Elapsed: 1 seconds
These packages failed to build:
ipsec-tools
Build Failed
Exiting on error or interrupt
looks like it can't find the file version.h. how can i fix this issue? Im a complete ltib noobm this is my first try to get it built.
thanks in advance
解決済! 解決策の投稿を見る。
It seems it depends on kernel to be build before it.
Checking the ipsec-tools recipe in Yocto it depends on kernel to be build, before building the recipe, check:
DESCRIPTION = "IPsec-Tools is a port of KAME's IPsec utilities to the \
Linux-2.6 IPsec implementation."
HOMEPAGE = "http://ipsec-tools.sourceforge.net/"
SECTION = "console/network"
LICENSE = "BSD"
DEPENDS = "virtual/kernel openssl readline flex"
It seems it depends on kernel to be build before it.
Checking the ipsec-tools recipe in Yocto it depends on kernel to be build, before building the recipe, check:
DESCRIPTION = "IPsec-Tools is a port of KAME's IPsec utilities to the \
Linux-2.6 IPsec implementation."
HOMEPAGE = "http://ipsec-tools.sourceforge.net/"
SECTION = "console/network"
LICENSE = "BSD"
DEPENDS = "virtual/kernel openssl readline flex"
Hi Otavio
Thank you very much for the hint.
I will definately try it today.
Does it works?
Hi Otavio
Im getting another error now, that ltib can't find version.h file.
I think there is a solution i've seen on google in regards to this, however, I'm thinking of focusing completely on yocto distro and use it instead since i keep hearing that freescale will switch to using yocto for all the next releases anyways
thank you for you help
Right; yes Yocto looks like a nicer option in my point of view :-)