Hello Freescale Community,
I have some trouble adding GPIO support on a i.MX28 Pin.
There is a two color LED on the Pins K4 and L4.
I'm using an 3.9 Kernel and it seems to run a Heartbeat on the LED on Pin K4.
I figured out with the file fsl,mxs-pinctrl.txt that the IDs are:
MX28_PAD_AUART1_RX__GPIO_3_4 0x3043
MX28_PAD_AUART1_TX__GPIO_3_5 0x3053
So I modified the imx28-evk.dts by copying something similar from the GPIO_3_5 to 3_4.
led_pin_gpio3_4: led_gpio3_4@0 {
reg = <0>;
fsl,pinmux-ids = <
0x3043 /* MX28_PAD_AUART1_RX__GPIO_3_4 */
>;
fsl,drive-strength = <0>;
fsl,voltage = <1>;
fsl,pull-up = <0>;
};
then I crosscompiled this dts to a dtb and attached it to the zImage
cat arch/arm/boot/zImage arch/arm/boot/dts/imx28-evk.dtb > arch/arm/boot/zImage_dtb
sudo cp arch/arm/boot/zImage_dtb ~/freescale/imx28/ltib/rootfs/boot/zImage
Now I tried to switch the LED GPIO on and off
Linux GPIO Number = <GPIO Instance – 1> × 32 + <GPIO Port number> = (3-1)*32+4 = 68
(found this formula here https://community.freescale.com/message/317413#317413 which document is the source?)
echo 68 >/sys/class/gpio/export
echo out >/sys/class/gpio/gpio68/direction
echo 1 >/sys/class/gpio/gpio68/value
echo 0 >/sys/class/gpio/gpio68/value
but the LED did not go on and off, have I forgot something?
已解决! 转到解答。
The formula you mentioned applies only to other i.mx devices, that starts counting the gpio from 1.
For mxs you should do: 3*32 + 4
This comes from the fact that mxs SoCs have 32 GPIOs per GPIO port and the hardware GPIOnumbering start from zero:
For example:
GPIO0_5 --> Linux number is 0*32 + 5
GPIO1_10 --> Linux number is 1*32 + 10
This differs from other i.mx, where we start counting from GPIO1, ie, there is no GPIO0 as per the SoC manual.
For example (there is no GPIO0 port on this family):
GPIO1_3 ---> Linux number (1-1)*32 + 3
GPIO3_7 ---> Linux number is (3-1)*32 + 7
Hope this helps to clarify why mxs and imx have different schemes to calculate the Linux gpio number.