Hello Community,
I've a question for routing the EMI_DDR_OPEN trace. If I read this right the appnote AN4215 says DDR_OPEN route length equals CLK routed length + DQS routet length. But there are 2 CLK traces (CLK and CLKn) and 4 DQS (DQS0, DQS0n, DQS1, DQS1n).
Do that mean I have to sum up the matched length of DQS and the matched length of CLK?
For Example_
DQM0 = 17,1 mm
DQM0n = 17,2 mm
DQM1 = 16,9 mm
DQM1n = 16,8 mm
CLK = 11,9mm
CLK = 12,1mm
Is now the length of EMI_DDR_OPEN (17+12)mm ?
thank You
已解决! 转到解答。
Thank you jimmychan,
I asked this question because I wondered that this formula doesn't work in the i.mx28 Design Files.
On this board I've measured:
CLK 12,3mm,
DQS0 17,4mm and
DQS1 17,1mm
with an EMI_DDR_OPEN = 35,6mm