i.MX RT1052 Processor的SEMC接口

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1052 Processor的SEMC接口

Jump to solution
1,051 Views
jiaxin
Contributor I

The SEMC interface supports 4 types of devices, I would like to confirm the following questions:

1. Does it support access two different devices through the SEMC interface in the same project, such as an external SDRAM plug-in, an external SRAM, and data interaction with two peripherals is required in the same project.

2. If it is supported, how much delay is there when the two devices are switched?

thankyou!

0 Kudos
Reply
1 Solution
1,016 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @jiaxin ,

1. Yes, 可以支持。他们的CS是不同的。数据线可能是复用的。

2. 这个很难讲。从一个cs起来到另一个落下大概需要3~4个clock。

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
2 Replies
1,017 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @jiaxin ,

1. Yes, 可以支持。他们的CS是不同的。数据线可能是复用的。

2. 这个很难讲。从一个cs起来到另一个落下大概需要3~4个clock。

 

Regards,

Jing

0 Kudos
Reply
1,027 Views
jiaxin
Contributor I

Hi,NXP

      Is there anyone who know answer?

0 Kudos
Reply