I have i.MX 8M Plus EVK Board and want to make some audio examples on it. I wanted to upgrade all packages in the system and run below command. After this command some warnings occured. Then I wanted to reboot by writing (reboot -h now). Normally It was resettable with that command but this time it did not reset. I manually reset it and it gives me kernel panic error while booting. What could be my mistake and how can I restore my system ? I had no change in EVK board's system so if it is easy I can go to initial status of the board.
#: apt-get dist-upgrade
Hello fozen,
Are you in yocto? you need implement this steps to do apt-upgarde:
1.Modify the build/conf/local.conf
2.Build our image
3.Generate the package index:
4.Run a webserver to expose package index to the outside world
5.Deploy the image to the target
6.Boot your target and update it
7.If you would like to install tcpdump/GStreamer. (don’t forget to update the package index as well)
Run the following on target
$ apt-get update
Regards