i.MX 8M Mini EVK boot mode switches

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini EVK boot mode switches

Jump to solution
1,096 Views
ranjithkumar_kv
Contributor II

Hi,

We are using i.MX 8M Mini Evk board. We have a confusion on the boot mode switches given in the Quick start guide and Silkscreen layer of the EVK board.

In Quick start guide it is given as to boot from eMMC we must change the boot switches of SW1101 to 0110110001 but in the silkscreen layer of the EVK board it is given as  0110110010. Attached the images below.

Even in Get Started with the i.MX 8M Mini EVK | NXP also the EVK board image given and the boot mode switches configuration provided seems to be contradicting.

So please let us know which is the correct configuration of boot mode switches to be enabled to boot the board from eMMC. Thanks in advance.

Regards,

Ranjith

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
987 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ranjith,

The emmc boot mode boot switches of SW1101 to 0110110001 is OK, you can refer to the user guide and schematic design.  Not the first picture you attached to me.

Have a nice day

Rita

View solution in original post

0 Kudos
Reply
2 Replies
988 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ranjith,

The emmc boot mode boot switches of SW1101 to 0110110001 is OK, you can refer to the user guide and schematic design.  Not the first picture you attached to me.

Have a nice day

Rita

0 Kudos
Reply
986 Views
ranjithkumar_kv
Contributor II

Hi Rita,

Thanks for your reply.

Regards,

Ranjith

0 Kudos
Reply