Hi, I'm trying to make an application which has the function play HEVC encoded 4K 60fps video stream on Android system.
But it becomes as below.
4K 24fps -> success
4K 60fps -> fail
Logcat told some frame droppings.
I tried to increase heap size of the system, but got same result.
It seems the problem is not a memory allocation.
I found a case which FFmpeg does not work correctly against V4L2 M2M option (specify hardware decoding) in 64-bit Raspberry Pi 4.
Could my case same to that?
CPU: i.MX 8M(Quad)
SoM: DART-MX8M
Media Player: LibVLC.Android 3.5.1
OS: Android 11
Best Regards,
已解决! 转到解答。
I have tested this with my download HEVC 4k@60fps on android 11_2.6.0 successfully, I want to test kernel 5.4.47 kernel (android 11_1.2.0), but refer to the release note, this version is only for i.MX 8M Plus (Silicon Revision A1) EVK Board and Platform, so I suggest that you can upgrade your android to the newer version
I try to play HEVC videos which are as below.
video name | size | fps | dynamic range | profile |
A | 4K | 24 | SDR | Main |
B | 4K | 60 | HDR | Main10 |
results on Yocto 3.0(kernel=5.4.24 using Gstreamer)
Gstreamer option:
gst-launch-1.0 -v filesrc location=<File Path> ! tsdemux ! h265parse ! vpudec ! autovideosink
results on Android 11(kernel=5.4.47 using VLC)
VLC option:
:codec=mediacodec_ndk,mediacodec_jni,all
Other video codec(H.264) is no problem.
Error logs of video B on Android is shown in the attachement.
I think It's something matter of during from the instruction of hardware decoding to the actual VPU behavior.
Regards,
I have tested this with my download HEVC 4k@60fps on android 11_2.6.0 successfully, I want to test kernel 5.4.47 kernel (android 11_1.2.0), but refer to the release note, this version is only for i.MX 8M Plus (Silicon Revision A1) EVK Board and Platform, so I suggest that you can upgrade your android to the newer version
It's very interesting. My EVK is not NXP's so the vendor may customize some settings for kernel 5.4.47.
Actually I already know a solution which can play this video by VPU. But this knowledge is very important that make my system more better.
Thank you for supporting.
Q. did you try other player on android?
It was failed on Cactus Player and Gstreamer.
But I tried two another Android devices(on VLC). All of them succeeded to play.
Q. pls share your video here
It is difficult because uploading is prohibited by the broadcasting law.
I'll find alternative videos which occurs the same problem.