i.MX 8M Family DDR Tool LPDDR4 32 Bit Bus Width Calibration Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Family DDR Tool LPDDR4 32 Bit Bus Width Calibration Error

Jump to solution
3,814 Views
onurcalili
Contributor I

Hello everyone,

 

We have designed a custom board with i.MX 8M Quad CPU. We controlled the voltages and clocks on the board. We are using "MT53B256M32D1NP" as LPDDR4 on board which is connected 32 bits bus width. Our boards MT53B256M32D1NP's layout information is given in attachment "ddr_specs.jpg" and DDR Controller Configuration Aid Spreadsheet configuration (RPA) based on MXM8M_LPDDR4_RPA_v24.xlsx is given in attachment "ddr_aid_cfg.jpg" and i.MX side connection schematic is given in attachment ddr_sch.jpg.

When we download the ds file to the board and then run calibration using DDR tool, the tool prints:

Downloading file 'bin\lpddr4_train1d_string.bin' ..Done

Downloading file 'bin\lpddr4_train2d_string.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_1d_imem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_1d_dmem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_2d_imem.bin' ..Done

Downloading file 'bin\lpddr4_pmu_train_2d_dmem.bin' ..Done

Downloading IVT header...Done
Downloading file 'bin\m850_ddr_stress_test.bin' ...Done

Download is complete
Waiting for the target board boot...

********Found PMIC PF0100**********

*************************************************************************

*************************************************************************

*************************************************************************
MX8 DDR Stress Test V3.10
Built on Feb 5 2020 14:08:44
*************************************************************************

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x91d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 800MHz
DDR Clock: 1600MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 15, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 1024MB
Density per controller is: 1024MB
Total density detected on the board is: 1024MB
============================================

MX8M: Cortex-A53 is found

*************************************************************************

============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1600Mhz...
[Process] End of CA training
[Process] End of initialization
PMU: Error: RxEn training preamble not found
PMU: ***** Assertion Error - terminating *****
[Result] FAILED

If we change the bus witdh to 16 using RPA then the calibration is done successfully but the density of DDR is shown as 512MB as expected. 

We could not found our problem. What causes "PMU: Error: RxEn training preamble not found" error? What can do after this point?  Any help appreciated. 

Best regards

Onur

0 Kudos
Reply
1 Solution
3,577 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

We have reviewed the your RPA and no problem is found.

From your description, there is something wrong in channel B of LPDDR4. Please go to check the hardware connection on LPDDR4 channel B.

View solution in original post

6 Replies
3,577 Views
onurcalili
Contributor I

Hi Rita,

Thank you very much for your help. By your help we see the problem. Our hardware guys had entered the symbology of DDR's channel pins in different order in DDR connections.

Thanks for your precious time.

Have a nice day.

0 Kudos
Reply
3,577 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome~~

0 Kudos
Reply
3,577 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Onur,

Could you send us your the customized Programming Aids, LPDDR4 datasheet and the DDR connection pictures. And then we will do further confirm it for you.

Have a nice day

Rita

0 Kudos
Reply
3,577 Views
onurcalili
Contributor I

Hi Rita,

Thank you for your interest.I am sorry to inform you that I can not share datasheet of MT53B256M32D1NP because of NDA concerns. But I think I can share the link of datasheet of MT53B256M32D1NP which is  "http://files.pine64.org/doc/datasheet/rockpro64/SM512M32Z01MD2BNP(200BALL).pdf ".

I am attaching the i.MX8MQ (m850) DDR Controller Configuration Spreadsheet that I customized. And the LPDDR4 connection pictures of the schematics of our board.

I can not attach the spreadsheet directly so I am sending the link that I shared the spreadsheet.

Filebin :: bin 2adcq1nmmh5q89pr 

Best regards.

Onur

IMX8M_LPDDR4.png

MT53B256M32D1NP-062AITCTR.png

0 Kudos
Reply
3,578 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

We have reviewed the your RPA and no problem is found.

From your description, there is something wrong in channel B of LPDDR4. Please go to check the hardware connection on LPDDR4 channel B.

3,577 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I will confirm it for you. Please wait.

0 Kudos
Reply