i.MX 7ULP EVK - Flashing issues with Android images

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 7ULP EVK - Flashing issues with Android images

Jump to solution
965 Views
shai_b
Senior Contributor II

Hello team,

I am trying to help my customer in bring up Android OS on our imx7ulp evk but without success.

I have follow through the guide (Document Number: AQSUG) and encountered an issue while trying to flash the pre-built image.

My working environment is Windows 10, when I have tried to run the following command in the powershell

. \ uuu_imx_android_flash.bat -f imx7ulp -m -e

I got the following error

This script is validated with uuu 1.2.135 version, please align with this version.

dtbo is supported

recovery is supported

imx7ulp-evk does not support emmc as a target device

change target device automatically

You do not have sufficient privilege to perform this operation.

Of course I made sure that I worked in download mode (SW1 - 01xx) and I am working with uuu for imx7 version 1.2.135 , BTW I didnt get any notification from the terminal to indicate that the board got into download mode.

Since I wish to work with a 16 gigabyte SD card and I am interested in working with HDMI as video output I tried the following command

 . \ uuu_imx_android_flash.bat -f imx7ulp -m -e -d evk -c 14

But still i get the same issue, Could you please guide me what i am doing wrong and if there is another way to flash android 9.0### OS on the development kit.

Waiting for your kind response, Thanks in advance.

Best Regards,

Shai

Labels (2)
0 Kudos
Reply
1 Solution
855 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Try to run cmd / powershell as administrator.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

1 Reply
856 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Try to run cmd / powershell as administrator.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.