i.MX 7 L4.1.0_1.1.0_GA BSP and Release Notes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 7 L4.1.0_1.1.0_GA BSP and Release Notes

Jump to solution
988 Views
falstaff
Senior Contributor I

Hi,


The i.MX Software and Development Tools website mentions "i.MX 7 L4.1.0_1.1.0_GA BSP release can support i.MX7D SABRE board." What release binaries is this sentence exactly referring to? I can't find any i.MX 7 related release on the Linux BSP page...

We mostly use the git trees directly as recommended, however, what I am looking for is the official release notes for the L4.1.0_1.1.0_GA BSP with regards to the i.MX 7 BSP (supported features etc.).

Best regards,

Stefan

Labels (3)
0 Kudos
1 Solution
563 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer L4.1.15 GA Linux Release, which supports the i.MX 6 family

and I.MX7 r1.1

i.MX 6 Series Software and Development Tool|NXP

Please use imx7dsabresd build configuration.

Support for i.MX7D R1.2 and i.MX7D EVK will be added soon (Jul).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
563 Views
falstaff
Senior Contributor I

Hi Yuri,

Thanks for the link. Found the release notes in fsl-yocto-L4.1.15_1.1.0-ga.tar.gz which notes of what is supported in i.MX 7.

Please use imx7dsabresd build configuration.

Ok, I guess that means there is no official binary release for i.MX7D EVK available yet?

Thanks

Stefan

0 Kudos
564 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer L4.1.15 GA Linux Release, which supports the i.MX 6 family

and I.MX7 r1.1

i.MX 6 Series Software and Development Tool|NXP

Please use imx7dsabresd build configuration.

Support for i.MX7D R1.2 and i.MX7D EVK will be added soon (Jul).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------