Hi,
I have a question about errata ERR009623 of i.MX 6D.
There two workarounds.
Either
- set Y stride line & UV stride to 16 bytes aligned when format is NI/PI 420/422 using SMFC
channel
or
- change the IDMAC burst size of the particular pixel formats from 32 pixels to 16 pixels
When it chose the first workaround, does Y stride line and UV stride mean the parameter of Stride Line SLY and SLUV in Table 37-14. Channel Parameters Memory for non-interleaved (continued) of i.MX6DQ reference manual?
Then, should these SLV and SLUV align 16 bytes when format is NI/PI 420/422?
Best Regards,
Sugiyama
Hello,
Your understanding of the Stride Line parameters is correct.
Note, the erratum is actual for i.MX 6DualPlus / 6QuadPlus only.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Yuri,
Thank you for the answer.
I understand it is for i.MX 6DQP only.
Best Regards,
Sugiyama