i.MX 6D ERR009623

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6D ERR009623

673 Views
sugiyamatoshihi
Contributor V

Hi,

I have a question about errata ERR009623 of i.MX 6D.

There two workarounds.

Either
- set Y stride line & UV stride to 16 bytes aligned when format is NI/PI 420/422 using SMFC
channel
or
- change the IDMAC burst size of the particular pixel formats from 32 pixels to 16 pixels

When it chose the first workaround, does Y stride line and UV stride mean the parameter of Stride Line SLY and SLUV in Table 37-14. Channel Parameters Memory for non-interleaved (continued) of i.MX6DQ reference manual?

Then, should these SLV and SLUV  align 16 bytes when format is NI/PI 420/422?

Best Regards,

Sugiyama

Labels (1)
0 Kudos
Reply
2 Replies

549 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Your understanding of the Stride Line parameters is correct.

  Note, the erratum is actual for i.MX 6DualPlus / 6QuadPlus only.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

549 Views
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thank you for the answer.

I understand it is for i.MX 6DQP only.

Best Regards,

Sugiyama

0 Kudos
Reply