[i.MAX6ULL] How to burn the imx6ull program after the fuse is broken

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[i.MAX6ULL] How to burn the imx6ull program after the fuse is broken

313 次查看
xisuisan
Contributor I

Hi,

   I was trying to use the secure boot feature recently and I've already broken fuse. And successfully signed uboot and zImage. And when we call hab_status and hab_auth_img to verify if a HAB Event was generated:

Secure boot enabled

HAB Confiquration: 0xfo. HAB state: 0x66

NO HAB Events Found!

   At this point I thought I had implemented secure boot, but then I ran into a problem. How do I use the tools to burn into device trees, filesystems, images? And do you need to manually write the certificate to fuse in production? Is there a quick way?

   I made some attempts with the documentation linked below.

https://boundarydevices.com/high-assurance-boot-hab-dummies/

Chapter: What about imx_usb_loader?

https://github.com/nxp-imx/mfgtools/wiki/UUU-default-support-protocol-list

Chapter: HABv4 closed chip support

https://community.nxp.com/t5/i-MX-Security/i-MX6UL-bootloader-code-signing-method-for-UUU-tool/ta-p/...

The links are probably all about using tools to modify the DCD region in uboot. After I follow this operation, I successfully burn uboot using imx_usb in ① but uboot will only be loaded once.

I think the reason uboot works here is because we're in the area where uboot is loaded:

---------------------------

succeeded (security 0x12343412, status 0x88888888)

jumping to 0x877ff400

-----------------------------

The content is as follows:

---------------------------

U-Boot 2021.04-dirty (Nov 08 2023-12:05:10 +0800)

 

CPU: i.MX6ULL rev1.1 528 MHz (running at 396 MHz)

CPU: Industrial temperature grade (-40C to 105C) at 47C

Reset cause: POR

Model: i.MX6 ULL 14x14 EVK Board

Board: MX6ULL 14x14 EVK

DRAM: 512 MiB

MMC: FSL_SDHC: 0, FSL_SDHC: 1

Loading Environment from MMC... *** Warning - bad CRC, using default environment

 

[*]-Video Link 0 (480 x 272)

[0] lcdif@21c8000, video

In: serial

Out: serial

Err: serial

switch to partitions #0, OK

mmc1(part 0) is current device

Net:

Warning: ethernet@20b4000 (eth1) using random MAC address - c2:81:d3:ec:bd:b3

eth1: ethernet@20b4000 [PRIME]Get shared mii bus on ethernet@2188000

 

Warning: ethernet@2188000 (eth0) using random MAC address - f6:e3:cd:25:16:87

, eth0: ethernet@2188000

Fastboot: Normal

Boot from USB for mfgtools

*** Warning - Use default environment for mfgtools

, using default environment

 

Run bootcmd_mfg: run mfgtool_args; if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..." ; fastboot 0; fi;

Hit any key to stop autoboot: 0

----------------------------

Once reset, uboot won't get up.

I put the uboot file with the modified DCD region into the mfgtool tool. If I do not modify the.imx file in fireware that is uboot, the mfgtool tool will be stuck in the jumping to OS section log below, see mfgtool1.log for details

-----------------------

...

CmdOperation[0] device chagned and reset to state 0

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is F:\driver_imax6ull\mfgtool\mfgtool\Profiles\linux\OS Firmware\firmware\u-boot-imx6ull-14x14-emmc.imx

---------------------------

After I replaced the imx file in fireware, the serial port was directly disconnected. For detailed log, please see mfgtool2.log

Finally, attached is the contents of the file I used cst tool. I suspect it has something to do with that, too

Maybe it's because my Engine option says SW, but if I use CAAM, DCP, or ANY, I get a HAB Event

标签 (1)
0 项奖励
回复
0 回复数