how to transcode MJPEG to H.264 on i.MX 8M Mini

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to transcode MJPEG to H.264 on i.MX 8M Mini

跳至解决方案
2,653 次查看
shengfazhang
Contributor II

Hi. I'm using i.MX 8M Mini to record video and capture image from camera. The video must support 1920X1080 60fps. I encountered some problem. 

1. If I use USB camera, we can get 1920X1080 60fps video stream. But the video format is MJPEG. So how can I use gstreamer with hardware acceleration (VPU) to transcode MJPEG to H.264 (save to file) ?

I use the following command. It seems that the jpegdec plugin is too slow! Is jpegdec hardware acceleration?

gst-launch-1.0 v4l2src device=/dev/video1 ! "image/jpeg,framerate=30/1,width=1920,height=1080" ! jpegparse ! jpegdec ! video/x-raw ! queue ! vpuenc_h264 ! filesink location=1080p.mp4 

2. If I use MIPI camera, we can only get 1920X1080 30fps video stream. The video format is YUYV. So I can use the following command:

gst-launch-1.0 -e v4l2src device=/dev/video0 io-mode=4 ! video/x-raw, format=YUY2, \
width=1920,height=1080, framerate=30/1 ! tee name=t ! queue ! vpuenc_h264 ! queue ! \
h264parse ! qtmux ! filesink location=test.mp4 t. ! queue ! waylandsink

So does i.MX8M Mini MIPI supports 1920X1080 60fps YUYV camera video stream? If so, is the above command fast enough (1080P 60fps)  to record the video stream to file?

If i.MX 8M Mini only supports 1920X1080 60fps MJPEG camera video stream by USB? How do I transcode MJPEG to H.264 and save to file by hardware acceleration (VPU) ?

Thank you!

标签 (1)
0 项奖励
回复
1 解答
2,643 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ZHANG

 

for franscoding one can look at sect.7.3.4 Transcoding   i.MX Linux User’s Guide​

I.MX8M Mini does not support in hardware mjpeg, vpu capabilities are described in

sect.13.1.1.3 Video Processing Unit (VPU)  i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,644 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ZHANG

 

for franscoding one can look at sect.7.3.4 Transcoding   i.MX Linux User’s Guide​

I.MX8M Mini does not support in hardware mjpeg, vpu capabilities are described in

sect.13.1.1.3 Video Processing Unit (VPU)  i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor

0 项奖励
回复
2,635 次查看
shengfazhang
Contributor II

Hi, igor.

Thanks for your kind reply. If I didn't misunderstand, i. MX 8M Mini doesn't support transcoding 1080P 60fps MJPEG format camera video stream to H.264 in real time as there is not such hardware. But it should support transcoding 1080P 60fps YUYV format camera video stream to H.264 by VPU. The gstreamer command should like the following:

gst-launch-1.0 -e v4l2src device=/dev/video0 io-mode=4 ! video/x-raw, format=YUY2, \
width=1920,height=1080, framerate=60/1 ! tee name=t ! queue ! vpuenc_h264 ! queue ! \
h264parse ! qtmux ! filesink location=test.mp4 t. ! queue ! waylandsink
0 项奖励
回复
2,630 次查看
igorpadykov
NXP Employee
NXP Employee

>But it should support transcoding 1080P 60fps YUYV format camera video stream to H.264 by VPU.

 

for such case one can look at sect.7.3.3 Video encoding  i.MX Linux User’s Guide​

 

Best regards
igor

0 项奖励
回复
2,614 次查看
shengfazhang
Contributor II

Hi, @igorpadykov. I want to use VPU Wrapper to encode the stream from camera directly. Is there any example for that? I just found some api doc and calling sequence in i.MX VPU Application Programming Interface Linux ® Reference Manual.

Thank you.

0 项奖励
回复
2,601 次查看
igorpadykov
NXP Employee
NXP Employee

in general one can look at vpu unit tests:

https://source.codeaurora.org/external/imx/imx-test/tree/test?h=lf-5.10.52_2.1.0

 

Best regards
igor

0 项奖励
回复