how to transcode MJPEG to H.264 on i.MX 8M Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to transcode MJPEG to H.264 on i.MX 8M Mini

ソリューションへジャンプ
2,654件の閲覧回数
shengfazhang
Contributor II

Hi. I'm using i.MX 8M Mini to record video and capture image from camera. The video must support 1920X1080 60fps. I encountered some problem. 

1. If I use USB camera, we can get 1920X1080 60fps video stream. But the video format is MJPEG. So how can I use gstreamer with hardware acceleration (VPU) to transcode MJPEG to H.264 (save to file) ?

I use the following command. It seems that the jpegdec plugin is too slow! Is jpegdec hardware acceleration?

gst-launch-1.0 v4l2src device=/dev/video1 ! "image/jpeg,framerate=30/1,width=1920,height=1080" ! jpegparse ! jpegdec ! video/x-raw ! queue ! vpuenc_h264 ! filesink location=1080p.mp4 

2. If I use MIPI camera, we can only get 1920X1080 30fps video stream. The video format is YUYV. So I can use the following command:

gst-launch-1.0 -e v4l2src device=/dev/video0 io-mode=4 ! video/x-raw, format=YUY2, \
width=1920,height=1080, framerate=30/1 ! tee name=t ! queue ! vpuenc_h264 ! queue ! \
h264parse ! qtmux ! filesink location=test.mp4 t. ! queue ! waylandsink

So does i.MX8M Mini MIPI supports 1920X1080 60fps YUYV camera video stream? If so, is the above command fast enough (1080P 60fps)  to record the video stream to file?

If i.MX 8M Mini only supports 1920X1080 60fps MJPEG camera video stream by USB? How do I transcode MJPEG to H.264 and save to file by hardware acceleration (VPU) ?

Thank you!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,644件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZHANG

 

for franscoding one can look at sect.7.3.4 Transcoding   i.MX Linux User’s Guide​

I.MX8M Mini does not support in hardware mjpeg, vpu capabilities are described in

sect.13.1.1.3 Video Processing Unit (VPU)  i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,645件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZHANG

 

for franscoding one can look at sect.7.3.4 Transcoding   i.MX Linux User’s Guide​

I.MX8M Mini does not support in hardware mjpeg, vpu capabilities are described in

sect.13.1.1.3 Video Processing Unit (VPU)  i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信
2,636件の閲覧回数
shengfazhang
Contributor II

Hi, igor.

Thanks for your kind reply. If I didn't misunderstand, i. MX 8M Mini doesn't support transcoding 1080P 60fps MJPEG format camera video stream to H.264 in real time as there is not such hardware. But it should support transcoding 1080P 60fps YUYV format camera video stream to H.264 by VPU. The gstreamer command should like the following:

gst-launch-1.0 -e v4l2src device=/dev/video0 io-mode=4 ! video/x-raw, format=YUY2, \
width=1920,height=1080, framerate=60/1 ! tee name=t ! queue ! vpuenc_h264 ! queue ! \
h264parse ! qtmux ! filesink location=test.mp4 t. ! queue ! waylandsink
0 件の賞賛
返信
2,631件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>But it should support transcoding 1080P 60fps YUYV format camera video stream to H.264 by VPU.

 

for such case one can look at sect.7.3.3 Video encoding  i.MX Linux User’s Guide​

 

Best regards
igor

0 件の賞賛
返信
2,615件の閲覧回数
shengfazhang
Contributor II

Hi, @igorpadykov. I want to use VPU Wrapper to encode the stream from camera directly. Is there any example for that? I just found some api doc and calling sequence in i.MX VPU Application Programming Interface Linux ® Reference Manual.

Thank you.

0 件の賞賛
返信
2,602件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

in general one can look at vpu unit tests:

https://source.codeaurora.org/external/imx/imx-test/tree/test?h=lf-5.10.52_2.1.0

 

Best regards
igor

0 件の賞賛
返信