Hello,
I see some people get imx53QSB support kernel 4.4.x and ubuntu16.04.1, I tried with my imx535QSB and make it boot up.
Almost every thing works except the snd card.
My question is: Does somebody try to use desktop rootfs on imx53 serial, or have a way to build new rootfs with kernel 4.x?
thanks!
Wenming
Hi igor,
Thanks for your reply. Yes the document helpful but linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga this one used kernel 2.6.x or it is 3.14.x?
Regards!
Wenming
Hi Wenming
one can check below guidleines, seems it may work for i.MX53 too
Installing Ubuntu Rootfs on NXP i.MX6 boards | NXP Community
For imx53QSB problems with kernel 4.4.x one can post on kernel mail list.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------