how to imx8mq-evk MIPI-Display + HDMI dual display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to imx8mq-evk MIPI-Display + HDMI dual display

1,983件の閲覧回数
kangmw086
Contributor III

hi.

i used i.mx8mq-evk and android8.1.

1. Can IMX8 use MIPI-Display and HDMI at the same time?

2. If possible, how should I modify it in kernel?

3. Is it possible to switch from Android APP to HDMI output while printing the screen with MIPI?

 

regards!

0 件の賞賛
返信
5 返答(返信)

1,979件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Please see i.mx8mq, there are settings zbout how to realize dual display.The dual display is show same content.

 

BR

Zhiming

 

 

0 件の賞賛
返信

1,966件の閲覧回数
kangmw086
Contributor III

Thank you for your reply.

Can't I use IMX8 HDMI directly?

Should it be used in MIPI + MIPI-DSI-to-HDMI format only?

I want to use IMX8 HDMI port right away.

I want to use IMX8 HDMI + MIPI-DSI...

 

regards.

0 件の賞賛
返信

1,961件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Of course you can use single display.Please see the quick user guide.Our bsp support single hdmi,single mipi,dual hdmi&mipi and dual hdmi.The MIPI-DSI TO HDMI just convert DSI data, you can use hdmi+mipi.Its  same setting.

 

BR

Zhiming

0 件の賞賛
返信

1,947件の閲覧回数
kangmw086
Contributor III

Like Quick start guide, u-boot gave the command, but it didn't work.

So I am modifying the kernel.

Should HDMI be operated in DCSS?
And can MIPI-Display be operated from lcdif?

I'm used I.MX8 and Android 8.1.

 

thanks.

0 件の賞賛
返信

1,958件の閲覧回数
kangmw086
Contributor III

Then can I print it out with MIPI and switch from Android Application to HDMI?

I want to implement MIPI and HDMI transitions into software.

And can I change the resolution using software?

Android confirmed resolution changes with the wm size 1280x700 command.

 

thank you.

0 件の賞賛
返信