how to enable eth0 in iMx8M mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to enable eth0 in iMx8M mini

978件の閲覧回数
mm2021
Contributor III

From the log, it seems that th ethernet driver is not inserted, how to enable eth0 in board iMx8M mini?

Do not want to change the root fs.

root@imx8mmab2:~# ifconfig eth0 up
[ 393.751339] fec 30be0000.ethernet eth0: Unable to connect to phy
ifconfig: SIOCSIFFLAGS: No such device

0 件の賞賛
返信
2 返答(返信)

971件の閲覧回数
mm2021
Contributor III

image file is image-imx8mmab2.sdcard, which is for i3d.

Thanks!

0 件の賞賛
返信

973件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

 

what bsp used in the case, one can check fec1 in dts:  &fec1 {.. status = "okay" :
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mm-evk.d...

 

Best regards
igor

0 件の賞賛
返信