My design requires to boot iMX8MN from uSDHC emmc 8-bit. As my understanding, the following settings are essential:
(1) BOOT_MODE_PIN = 0010b ---> uSDHC3 emmc 8-bit as boot device
(2) OCOTP_BOOT_CFG0 = 0x0000_0a00 ---> override uSDHC with uSDHC1 emmc
My question: do the fuse bits in BOOT_CFG0 register become valid without BT_FUSE_SEL blown?
Thanks in advance!
BR
Cheng Shi
已解决! 转到解答。
uSDHC1 boot implemented with following settings:
(1) CFG pins configured as uSDHC3(emmc) boot mode
(2) eFuse.470 => 0x0000_2a000 to override to uSDHC1 boot
The important point is keeping BT_FUSE_SEL un-burn, so that manufacture SD2 boot can be triggered by changing CFG pins settings, which is required in boot image update.
Yes, 0x470[15:0] BOOT_CFG 16 BOOT configuration register, Usage varies, depending on selected boot device. And BT_FUSE_SEL is Determines, whether using fuses for boot configuration, or GPIO /Serial loader.
uSDHC1 boot implemented with following settings:
(1) CFG pins configured as uSDHC3(emmc) boot mode
(2) eFuse.470 => 0x0000_2a000 to override to uSDHC1 boot
The important point is keeping BT_FUSE_SEL un-burn, so that manufacture SD2 boot can be triggered by changing CFG pins settings, which is required in boot image update.