Hi I'm developing with imx28 (i.MX28) platform. BSP version is L2.6.35_10.12.01.
I'd like to access gpio port on user space.
So I did configuration of kernel. And I checked config file that show the flag "CONFIG_GPIO_SYSFS=y".
But I can't see the sysfs on /sys/class/gpio. This is my NFS mounted directory of Ubuntu host.
root@freescale /sys/class$ ls
backlight input net scsi_device vc
bdi leds power_supply scsi_disk video4linux
block mdio_bus raw scsi_host vtconsole
bsg mem rc sound
firmware misc regulator spi_master
graphics mmc_host rfkill tty
i2c-adapter mtd rtc ubi
After the configuration I rebuild the image. The image name rebuilt is rootfs.ext2.gz.
This is copy to NFS directory (/tools/rootfs).
Can anybody tell me how to access /sys/class/gpio sysfs.
Thanks.
Solved! Go to Solution.
I solved this.
At first I say thanks to Yuri Muhin and Emanuele Coli answer (https://community.freescale.com/message/312813#312813).
apply the configuration CONFIG_GPIO_SYSFS=y
after build the image(uImage) and update tftp directory.
and then you will see the /sys/class/gpio sysfs.
change the source code /arch/arm/mach-mx28/mx28evk_pins.c In my case
{
.name = "SSP0_DATA4",
.id = PINID_SSP0_DATA4,
.fun = PIN_GPIO,
.strength = PAD_4MA,
.voltage = PAD_3_3V,
.pullup = 1,
.drive = 1,
.pull = 1,
.data = 1,
.output = 1,
},
and after modify the source code call the gpio_export function like as.
status = gpio_request(MXS_PIN_TO_GPIO(PINID_SSP0_DATA4), "GPS_RESET");
/* already requested ? */
if (status == -EBUSY) {
gpio_export(MXS_PIN_TO_GPIO(PINID_SSP0_DATA4), false);
}
In my case without this I can't see /sys/class/gpio/gpioXX.
root@freescale /sys/class/gpio$ ls
export gpiochip0 gpiochip32 gpiochip96
gpio68 gpiochip128 gpiochip64 unexport
Now I can change the value on GPIO using this command.
root@freescale /module_test$ echo 0 > /sys/class/gpio/gpio68/value
root@freescale /module_test$ echo 1 > /sys/class/gpio/gpio68/value
I did verify that with Oscilloscpe. I hope this report make a help to others.
Thanks.
I solved this.
At first I say thanks to Yuri Muhin and Emanuele Coli answer (https://community.freescale.com/message/312813#312813).
apply the configuration CONFIG_GPIO_SYSFS=y
after build the image(uImage) and update tftp directory.
and then you will see the /sys/class/gpio sysfs.
change the source code /arch/arm/mach-mx28/mx28evk_pins.c In my case
{
.name = "SSP0_DATA4",
.id = PINID_SSP0_DATA4,
.fun = PIN_GPIO,
.strength = PAD_4MA,
.voltage = PAD_3_3V,
.pullup = 1,
.drive = 1,
.pull = 1,
.data = 1,
.output = 1,
},
and after modify the source code call the gpio_export function like as.
status = gpio_request(MXS_PIN_TO_GPIO(PINID_SSP0_DATA4), "GPS_RESET");
/* already requested ? */
if (status == -EBUSY) {
gpio_export(MXS_PIN_TO_GPIO(PINID_SSP0_DATA4), false);
}
In my case without this I can't see /sys/class/gpio/gpioXX.
root@freescale /sys/class/gpio$ ls
export gpiochip0 gpiochip32 gpiochip96
gpio68 gpiochip128 gpiochip64 unexport
Now I can change the value on GPIO using this command.
root@freescale /module_test$ echo 0 > /sys/class/gpio/gpio68/value
root@freescale /module_test$ echo 1 > /sys/class/gpio/gpio68/value
I did verify that with Oscilloscpe. I hope this report make a help to others.
Thanks.
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		General consideration are as following.
 
 Although you can develop your own driver to control GPIOs inside kernel space, there is a much simpler way for accessing GPIOs from user space. When timing requirements are not an issue, you are able to use GPIO-SYSFS.  SYSFS is a virtual file system that exports some kernel internal framework functionalities to user space and GPIO is one of the frameworks that can have functionalities exported through SYSFS.
The GPIO-SYSFS feature is available in all mainline kernels from 2.6.27 onwards.
Configuring Kernel to export GPIO through SYSFS
To enable GPIO in SYSFS, select the following kernel option:
Device Drivers --->
--- GPIO Support
[*] /sys/class/gpio/... (sysfs interface)
If you are using i.MX233 or i.MX28, after recompiling the kernel, do not forget to generate boot streams again,
because this is not automatic even in ltib. Be sure that the pins you will try to use are really accessible as GPIO pins
and were not requested by the kernel (gpio_request). If pin was gpio_request'ed, you will need to gpio_export the same
pin inside the kernel in order to have it accessible through SYSFS. If pin is not set as GPIO by default, you will need to set
IO MUX in the proper file inside <kernel>/arch/arm/mach-XXX. For i.MX28 EVK this is
 <ltib_dir>/rpm/BUILD/linux/arch/arm/mach-mx28/mx28evk_pins.c  
Accessing GPIO in user space
After enabling GPIO-SYSFS feature, you can boot your device with the new kernel to make some tests.
First you need to export the GPIO you want to test to the user space:
echo XX > /sys/class/gpio/export
XX shall be determined by the following algorithm:
GPIOA_[B] is the GPIO you want to export, where "A" is the GPIO bank and "B" is the offset of the pin in the bank.
if the first available GPIO bank is 0 // (iMX.28, for example)
XX = A*32 + B;
else // first GPIO bank is 1
XX = (A-1)*32 + B;
After exporting a GPIO pin, you shall be able to see the GPIO interface exported to:
/sys/class/gpio/gpioXX
Through this interface, you are now able to do things like:
# Reading the pin value
cat /sys/class/gpio/gpioXX/value
# Changing pin direction
echo in > /sys/class/gpio/gpioXX/direction
echo out > /sys/class/gpio/gpioXX/direction
# Toggling GPIO output level
echo 0 > /sys/class/gpio/gpioXX/value
echo 1 > /sys/class/gpio/gpioXX/value
It is important to note that through the GPIO virtual filesystem it is only possible to deal with
one GPIO pin at a time (per command).
Thank you Yuri.
I did Kernel Configuration for GPIO. I checked in configuration files in ./config directory.
ykmin@ubuntu:~/L2.6.35_10.12.01_ER_source/LTIB/ltib$ grep -rwn "CONFIG_GPIO_SYSFS" ./config
./config/platform/imx/imx28evk_updater_defconfig.dev:853:# CONFIG_GPIO_SYSFS is not set
./config/platform/imx/imx28evk_defconfig.dev:1077:CONFIG_GPIO_SYSFS=y
I did rebuild the image ./ltib -f command. (Is this right?)
I don't modify yet in <ltib_dir>/rpm/BUILD/linux/arch/arm/mach-mx28/mx28evk_pins.c
Rebuilded image (rootfs.ext2.gz) copy to NFS directory (/tools/rootfs).
I connect my board to NFS directory and I check if /sys/class/gpio sysfs. But not founded.
Can you tell me what mean you tell me.
If pin was gpio_request'ed, you will need to gpio_export the same
pin inside the kernel in order to have it accessible through SYSFS.
Thank you.