我尝试各种办法,wm8960始终不能得到声音输出。调试过程如下:
首先,打开电源使能脚:
ret=gpio_request(SABRESD_CODEC_PWR_EN, "audio_pwr_en");
if (!ret){
printk("Turn on audio(wm8962) power!(1:enable)\n");
gpio_direction_output(SABRESD_CODEC_PWR_EN, 1); // 0:enable, 1:disable
gpio_free(SABRESD_CODEC_PWR_EN);
}
串口打印如下出错信息:
wm8962 0-001a: Failed to get supply 'SPKVDD1': -19
wm8962 0-001a: Failed to request supplies: -19
wm8962 0-001a: asoc: failed to probe CODEC wm8962.0-001a: -19
asoc: failed to instantiate card wm8962-audio: -19
Initialize HDMI-audio failed. Load HDMI-video first!
ALSA device list:
No soundcards found.
把imx6q_init_audio();后移几行,上面的错误就没有了。但出现下面错误 :
wm8962 0-001a: Device is not a WM8962, ID 0 != 6243
wm8962 0-001a: asoc: failed to probe CODEC wm8962.0-001a: -22
asoc: failed to instantiate card wm8962-audio: -22
把sound/soc/codec/下面的wm8962.c改用wm8960.c(修改Kconfig和Makefile)。
wm8960_i2c_probe不调用。原因是:
.driver = {
.name = "wm8960",
而 {
I2C_BOARD_INFO("wm8962", 0x1a),
.platform_data = &wm8962_config_data,
},
linux driver是根据name来匹配的,如果匹配就调用。
登记了snd_soc_register_codec后,codec的probe也不调用。
原因是下面这个snd_dai_driver的name要一致才能调用。
static struct snd_soc_dai_driver wm8960_dai = {
.name = "wm8960",
static struct snd_soc_dai_link imx_dai[] = {
{
.name = "HiFi",
.stream_name = "HiFi",
.codec_dai_name = "wm8960",
调用后显示:
wm8960 0-001a: wm8960 probed success!
wm8960 0-001a: Failed to add route HPOUTL->Headphone Jack
asoc: wm8960 <-> imx-ssi.1 mapping ok
input: wm8960-audio DMIC as /devices/platform/soc-audio.5/sound/card0/input1
input: wm8960-audio Ext Spk as /devices/platform/soc-audio.5/sound/card0/input2
ALSA device list:
#0: wm8960-audio
root@imx6solo ~$ find / -name *wm8960*
/sys/devices/platform/imx-wm8960.0
/sys/bus/platform/devices/imx-wm8960.0
/sys/bus/platform/drivers/imx-wm8960
/sys/bus/platform/drivers/imx-wm8960/imx-wm8960.0
/sys/bus/i2c/drivers/wm8960
/proc/asound/wm8960audio
root@imx6solo ~$
问题是/dev/下面并没有增加设备,无法使用/dev/pcm。
root@imx6solo /usr/bin$ aplay -L
null
Discard all samples (playback) or generate zero samples (capture)
root@imx6solo /usr/bin$ aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: wm8960audio [wm8960-audio], device 0: HiFi wm8960-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
root@imx6solo /usr/bin$
现在应该是试试ALSA驱动程序是不是真能用的时候了. 接者就是使用它.
查看声卡是否存在:
root@imx6solo ~$ cat /proc/asound/cards
0 [wm8960audio ]: wm8960-audio - wm8960-audio
wm8960-audio
ALSA 驱动程序在 /dev/snd/ 目录下有自己的驱动程序。
root@imx6solo ~$ ls /dev/snd/
controlC0 pcmC0D0c pcmC0D0p timer
http://www.alsa-project.org/main/index.php/Download上面下载alsa tester包括alsa-lib, alsa-utils。
编译:./gitcompile CC=arm-linux-gcc --host=arm-linux
现在进化到configure都从网络上临时下载的地步了,我有点out了。
编译alsa-utils总是过不去。重新下载alsaplayer。
./configure --host=arm-linux CC=arm-linux-gcc --disable-oggvorbis
然后make.
对比了wm8960.c/wm8962.c, imx-wm8960.c/imx-wm8962.c,差别其实非常大。
http://bbs.21ic.com/forum.php?mod=viewthread&tid=869393,从这个链接地址可以下载imx-wm8960.c。
重新配置linux kernel,设备/dev/dsp和/dev/mixer出来,这是OSS接口的要求。
root@imx6solo /test/audio$ ./wavplay test.wav
-------------------------------------------------------------------->
File Magic: [RIFF]
File Length: [424636]
File Type: [WAVE]
Fmt Magic: [fmt ]
Fmt Size: [16]
Fmt Format: [PCM]
Fmt Channels: [2]
Fmt Sample_rate: [22050](HZ),22khz
Fmt Bytes_p_second: [88200]
Fmt Blocks_align: [4]
Fmt Sample_length: [16]
Chunk Type: [data]
Chunk Length: [424600]
<--------------------------------------------------------------------
Plug PCM: Rate conversion PCM (44100, sformat=S16_LE)
Converter: linear-interpolation
Protocol version: 10002
Its setup is:
stream : PLAYBACK
access : RW_INTERLEAVED
format : S16_LE
subformat : STD
channels : 2
rate : 22050
exact rate : 22050 (22050/1)
msbits : 16
buffer_size : 8192
period_size : 256
period_time : 11609
tstamp_mode : NONE
period_step : 1
avail_min : 256
period_event : 0
start_threshold : 1
stop_threshold : 8192
silence_threshold: 0
silence_size : 0
boundary : 536870912
Slave: Direct Stream Mixing PCM
Its setup is:
stream : PLAYBACK
access : MMAP_INTERLEAVED
format : S16_LE
subformat : STD
channels : 2
rate : 44100 //44khz
exact rate : 44100 (44100/1)
msbits : 16
buffer_size : 16384
period_size : 512
period_time : 11609
tstamp_mode : NONE
period_step : 1
avail_min : 512
period_event : 0
start_threshold : 2
stop_threshold : 16384
silence_threshold: 0
silence_size : 0
boundary : 1073741824
Hardware PCM card 0 'wm8960-audio' device 0 subdevice 0
Its setup is:
stream : PLAYBACK
access : MMAP_INTERLEAVED
format : S16_LE
subformat : STD
channels : 2
rate : 44100 //44khz
exact rate : 44100 (44100/1)
msbits : 16
buffer_size : 16384
period_size : 512
period_time : 11609
tstamp_mode : ENABLE
period_step : 1
avail_min : 512
period_event : 0
start_threshold : 1
stop_threshold : 1073741824
silence_threshold: 0
silence_size : 1073741824
boundary : 1073741824
appl_ptr : 0
hw_ptr : 0
root@imx6solo /test/audio$ aplay test.wav
Playing WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 22050 Hz, Stereo
Aborted by signal Interrupt...
root@imx6solo /test/audio$
仍然是没有声音输出!!
换了一个44khz采集率的wav文件,仍然没有声音输出!
root@imx6solo /test/audio$ aplay xihuanni.wav
Playing WAVE 'xihuanni.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
Aborted by signal Interrupt...
再次检查了pin mux config,是正确的。但就是没有任何audio输出!
如果直接用imx-wm8962.c,则有许多出错信息,如下:
root@imx6solo /test/audio$ aplay xihuanni.wav
WM8960 PLL: Unsupported N=3
Failed to start FLL: -22
Failed to set SYSCLK: -22
asoc: machine hw_params failed
Failed to set SYSCLK: -22
ALSA lib pcm_direct.c:980:(snd1_pFailed to set SYSCLK: -22
cm_direct_initialize_slave) unable to install hw params
ALSA lib pcm_dmix.c:1030:(snd_pcm_dmix_open) unable to initialize slave
aplay: main:660: audio open error: Invalid argument
所以,要用imx-wm8962.c来修改的话,还有点麻烦,不会很容易。
网上找了一个人交流,他用的是imx-wm8960.module,就是编译出来的.o
ifneq ($(wildcard sound/soc/imx/imx-wm8960.c),)
snd-soc-imx-wm8960-objs := imx-wm8960.c
else
snd-soc-imx-wm8960-objs := imx-wm8960.module
endif
我这样修改后,运行导致crash。
register wm8960 I2C driver success!
Unable to handle kernel paging request at virtual address f8f2fe18
pgd = 80004000
[f8f2fe18] *pgd=1bce9811, *pte=00000000, *ppte=00000000
Internal error: Oops: 807 [#1] PREEMPT
Modules linked in:
CPU: 0 Not tainted (3.0.101-2790-gc248ed7 #274)
Hi yingcai Tan,
Which version of BSP are you using?
Have a great day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
e.g. if you using AUD3 pins (TXC, TXFS, TXD, RXD...) , make sure the IOMUX setting properly in the your_board.c file.
Also, please check the AUD3 PAD setting is properly in the linux/arch/arm/plat-mxc/include/mach/iomux-mx6dl.h.
For example: if the PAD setting is NO_PAD_CTRL for the pins, please change it to MX6DL_ADU_PAD_CTRL.
#define MX6DL_PAD_CSI0_DAT5__AUDMUX_AUD3_TXD \
IOMUX_PAD(0x038C, 0x0078, 4, 0x0000, 0, NO_PAD_CTRL)
change to :
#define MX6DL_PAD_CSI0_DAT5__AUDMUX_AUD3_TXD \
IOMUX_PAD(0x038C, 0x0078, 4, 0x0000, 0, MX6DL_ADU_PAD_CTRL)
I double checked, see below:
#define MX6DL_PAD_CSI0_DAT7__AUDMUX_AUD3_RXD | \ |
IOMUX_PAD(0x0394, 0x0080, 4, 0x0000, 0, MX6DL_ADU_PAD_CTRL) |
#define MX6DL_PAD_CSI0_DAT6__AUDMUX_AUD3_TXFS | \ |
IOMUX_PAD(0x0390, 0x007C, 4, 0x0000, 0, MX6DL_ADU_PAD_CTRL) |
#define MX6DL_PAD_CSI0_DAT7__AUDMUX_AUD3_RXD | \ |
IOMUX_PAD(0x0394, 0x0080, 4, 0x0000, 0, MX6DL_ADU_PAD_CTRL) |
#define MX6DL_PAD_CSI0_DAT6__AUDMUX_AUD3_TXFS | \ |
IOMUX_PAD(0x0390, 0x007C, 4, 0x0000, 0, MX6DL_ADU_PAD_CTRL) |
Still no audio out.
More info:
root@imx6solo /test/audio$ aplay xihuanni.wav
snd_pcm_dmix_open()
imx_ssi_startup
snd1_pcm_hw_open_fd()
imx_ssi_set_dai_fmt,ret=0
*** sample_rate = 44100, bclk = 24000000, sysclk = 11289600
imx_ssi_hw_params
snd_imx_pcm_mmap,ret=0
imx_ssi_trigger,ret=0
snd_pcm_plug_open()
Playing WAVE 'xihuanni.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
snd_pcm_mmap_writei
Aborted by signal Interrupt...imx_ssi_trigger,ret=0
imx_ssi_shutdown
root@imx6solo /test/audio$
pls check attachment.
在 2015-04-23 16:19:39,jimmychan <admin@community.freescale.com> 写道:
|
|
|
|
Re: help: imx6solo wm8960始终没有声音输出
reply from jimmychan in i.MX Community - View the full discussion
is there any signal output from the AUDMUX pins? could you show me the part of schematic how you connect the wm8960?
Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread! |
Reply to this message by replying to this email, or go to the message on Freescale Community |
Start a new discussion in i.MX Community by email or at Freescale Community |
Following Re: help: imx6solo wm8960始终没有声音输出 in these streams: Inbox |
|
|
我怀疑是软件原因:
在static int imx_ssi_probe(struct platform_device *pdev)中,
ret = snd_soc_register_dai(&pdev->dev, dai);
if (ret) {
dev_err(&pdev->dev, "register DAI failed\n");
goto failed_register;
}
而在static __devinit int wm8960_i2c_probe(struct i2c_client *i2c,
const struct i2c_device_id *id)中,
ret = snd_soc_register_codec(&i2c->dev,
&soc_codec_dev_wm8960, &wm8960_dai, 0);
Registered DAI 'wm8960-hifi'
Registered DAI 'imx-ssi.1'
设置audio参数时,imx_hifi_hw_params()中调用的是wm8960-hifi的DAI驱动。
现在的问题是SSI的imx_ssi_set_dai_sysclk()或imx_ssi_set_dai_sysclk()都无法调用,我不知道这是否是SSI的BCLK无信号的原因。
Please check if you are mapping the Speaker with dapm widget correctly. For example, in the imx_wm8962_init, there are Headphone and AMIC. And there are some codes are checking the hp_gpio which is the Headphone Detect gpio pin. But in your schematic, you don't use the headphone. So, please check your driver code, the speaker may not map correctly.
I've masked the detect pin already. I put code here.
static int mxc_wm8962_init(void)
{
int rate;
clko = clk_get(NULL, "clko_clk");
if (IS_ERR(clko)) {
pr_err("can't get CLKO clock.\n");
return PTR_ERR(clko);
}
/* both audio codec and comera use CLKO clk*/
rate = clk_round_rate(clko, 24000000);
clk_set_rate(clko, rate);
wm8962_data.sysclk = rate;
return 0;
}
static struct mxc_audio_platform_data wm8962_data = {
.ssi_num = 1,
.src_port = 2,
.ext_port = 3,
// .hp_gpio = SABRESD_HEADPHONE_DET,
.hp_active_low = 1,
// .mic_gpio = SABRESD_MICROPHONE_DET,
.mic_active_low = 1,
.init = mxc_wm8962_init,
.clock_enable = wm8962_clk_enable,
};
在 2015-04-24 13:37:36,jimmychan <admin@community.freescale.com> 写道:
|
|
|
|
help: imx6solo wm8960始终没有声音输出
reply from jimmychan in i.MX Community - View the full discussion
Please check if you are mapping the Speaker with dapm widget correctly. For example, in the imx_wm8962_init, there are Headphone and AMIC. And there are some codes are checking the hp_gpio which is the Headphone Detect gpio pin. But in your schematic, you don't use the headphone. So, please check your driver code, the speaker may not map correctly.
Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread! |
Reply to this message by replying to this email, or go to the message on Freescale Community |
Start a new discussion in i.MX Community by email or at Freescale Community |
Following help: imx6solo wm8960始终没有声音输出 in these streams: Inbox |
|
|
I mean in the sound/soc/imx/imx-wm8962.c , not the board-mx6q_sabresd.c.
You can find the "plat->hp_gpio" in the code.
and the "if (plat->hp_gpio != -1)"
So, if you comment out the hp_gpio in board-mx6q_sabresd.c, then hp_gpio become -1, that may be the problem.
And could you kindly provide me imx-wm8960.c ? thanks.
在 2015-04-24 14:30:35,jimmychan <admin@community.freescale.com> 写道:
|
|
|
|
help: imx6solo wm8960始终没有声音输出
reply from jimmychan in i.MX Community - View the full discussion
I mean in the sound/soc/imx/imx-wm8962.c , not the board-mx6q_sabresd.c.
You can find the "plat->hp_gpio" in the code.
and the "if (plat->hp_gpio != -1)"
So, if you comment out the hp_gpio in board-mx6q_sabresd.c, then hp_gpio become -1, that may be the problem.
Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread! |
Reply to this message by replying to this email, or go to the message on Freescale Community |
Start a new discussion in i.MX Community by email or at Freescale Community |
Following help: imx6solo wm8960始终没有声音输出 in these streams: Inbox |
|
|
sorry, I don't have imx-wm8960.c.
please check in your driver code, please try to add the widget and audio_map for the speaker. And enable the speaker in the imx_wm8960_init.
For reference,
But I use imx-wm8960.c which does not check plat->hp_gpio
在 2015-04-24 14:30:35,jimmychan <admin@community.freescale.com> 写道:
|
|
|
|
help: imx6solo wm8960始终没有声音输出
reply from jimmychan in i.MX Community - View the full discussion
I mean in the sound/soc/imx/imx-wm8962.c , not the board-mx6q_sabresd.c.
You can find the "plat->hp_gpio" in the code.
and the "if (plat->hp_gpio != -1)"
So, if you comment out the hp_gpio in board-mx6q_sabresd.c, then hp_gpio become -1, that may be the problem.
Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread! |
Reply to this message by replying to this email, or go to the message on Freescale Community |
Start a new discussion in i.MX Community by email or at Freescale Community |
Following help: imx6solo wm8960始终没有声音输出 in these streams: Inbox |
|
|