hdmi display shows unexpected black block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hdmi display shows unexpected black block

814 Views
conteczxy
Contributor III

I am developing on imx6q custom board with android 4.4.2, kernel 3.0.35, the board is connected with hdmi ( 1920x1080M@60 )

I met a problem, when android is running, some black block will show on the screen, its position is uncertain, and its shape is not fixed, some pixel dot or some pixels serial dots will be black.

I exec the screenshot, and the output image is the same as we see on the screen, so I think the hardware is OK. because the graphic framebuffer is also with black block.

Anyone met the same problem?

Any suggestion is appreciated.

Thanks.

The following image is part of screen containing the black block.

pastedImage_6.png

Labels (3)
Tags (2)
1 Reply

616 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Since screenshot has the same issue, it should be caused by uplayer code, it is not the low level driver issue.

Maybe you need check your code modification in Android framework to identify which caused the issue.