I am trying to videoscale my video but with no success. the command i use
gst-launch-1.0 -vv v4l2src ! video/x-raw,width=720,height=576 ! queue ! videoscale ! video/x-raw,width=1024,height=720 ! waylandsink
i see the the videoscale is happening but just before the output there is another videoscale to the original scale.
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, width=(int)720, height=(int)576, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)be
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, width=(int)720, height=(int)576, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(ste
/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, width=(int)720, height=(int)576, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt70e
/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, width=(int)720, height=(int)576, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(string)bt70e
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, width=(int)720, height=(int)576, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(se
/GstPipeline:pipeline0/GstVideoScale:videoscale0.GstPad:src: caps = video/x-raw, width=(int)1024, height=(int)720, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)225/256, colorimetre
/GstPipeline:pipeline0/GstCapsFilter:capsfilter1.GstPad:src: caps = video/x-raw, width=(int)1024, height=(int)720, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)225/256, colorimetre
/GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, width=(int)1024, height=(int)720, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)225/256, colorime
/GstPipeline:pipeline0/GstCapsFilter:capsfilter1.GstPad:sink: caps = video/x-raw, width=(int)1024, height=(int)720, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)225/256, colorimete
/GstPipeline:pipeline0/GstVideoScale:videoscale0.GstPad:sink: caps = video/x-raw, width=(int)720, height=(int)576, format=(string)YUY2, framerate=(fraction)50/1, pixel-aspect-ratio=(fraction)1/1, colorimetry=(se
Why does the videoscale not stay as in the command?
hi joanxie
from reading the gst-inspect on imxvideoconvert_g2d i could not find any resize or resolution change option. there is format converting or rotation but not resizing. if you could send me an example how to resize with imxvideoconvert_g2d that will be great
i also tried the render-rectangle with no success.
thanks
Ran
hi joanxie
from reading the gst-inspect on imxvideoconvert_g2d i could not find any resize or resolution change option. there is format converting or rotation but not resizing. if you could send me an example how to resize with imxvideoconvert_g2d that will be great
i also tried the render-rectangle with no success.
thanks
Ran
refer to the linux user guide,
Resize
gst-launch-1.0 videotestsrc ! video/x-raw,format=NV12,width=800,height=600 ! imxvideoconvert_{xxx} !
video/x-raw, width=640, height=480 ! ximagesink display=:0
for imxvideoconvert_{xxx}, you can use imxvideoconvert_g2d
thanks for the reply
the imxvideoconverte_g2d works with the ximagesink. the problem is that it uses 80% of CPU. is there an option to use the waylandsink or glimagesink to handle this kind of convertions?
also if seems that i made also an error in the explanation. it seems that the video is in all of the screen but has large black borders on the side as if to fix the aspect-ratio.
could there be a solution using the wayland or glimage, that use the gpu and not the cpu, to stretch the width to full screen, or all the stretching and converting can be done only on the ximagesink with the cpu?
thanks
Ran
you can change it to the waylandsink, do you test it? the command I sent to you just for reference, you can change it as your demands, if you want to capture full screen video from camera, you can try the command like:
gst-launch-1.0 v4l2src ! video/x-raw,width=640,height=480 ! waylandsink