gstreamer video at 720p and 25/30 fps

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gstreamer video at 720p and 25/30 fps

ソリューションへジャンプ
4,969件の閲覧回数
philippeballeyd
Contributor IV

Hi everyone

i'm trying to stream over the network a USB webcam. I previously manage to do so at 1280x720 with 10 fps but couldn't get to 25 or 30 fps because the camera wasn't powerful enough. So i bought a new USB camera (Logitech C920) wich is able to do 720p at 30fps (as the documentation says)

The problem is that it is still not working for 25 or 30fps

Here are the gstreamer commands i'm using:

Sender:

gst-launch v4l2src device=/dev/video0 ! video/x-raw-yuv,width=1280,height=720,framerate=10/1 ! ffmpegcolorspace ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.20.27 port=5000 

Receiver:

gst-launch udpsrc port=5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, payload=(int)96, encoding-name=(string)H264" ! rtph264depay ! ffdec_h264 ! xvimagesink 

So this is working at 10fps. When i try to change to more fps, it fails with the following error:

Setting pipeline to PAUSED ...

[INFO] Product Info: i.MX6Q/D/S

vpuenc versions

plugin: 3.0.11

wrapper: 1.0.46(VPUWRAPPER_ARM_LINUX Build on Sep 29 2014 16:56:55)

vpulib: 5.4.23

firmware: 3.1.1.46056

ERROR: Pipeline doesn't want to pause.

ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Could not negotiate format

Additional debug info:

/media/philippe/data/fsl-release-bsp/build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer/0.10.36-r3/gstreamer-0.10.36/libs/gst/base/gstbasesrc.c(2830): gst_base_src_start (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:

Check your filtered caps, if any

Setting pipeline to NULL ...

Freeing pipeline ...

If i delete the width parameter, i get up to 15fps but not more. As the error states, it could not negotiate format. So i believe i have to change/add/remove the "video/x-raw-yuv,width=1280,height=720,framerate=10/1" parameter. But what should i change to make it works?

PS: if i plug my USB webcam to my computer, i manage to record 720@25fps with VLC without any problems

PS2: When i add the plugin videorate to my gstreamer command, it gets really laggy (less than a frame per second), but it seems it is not due to CPU usage, since it remains the same

Any pointers would be of great help Smiley Wink

Thanks

ラベル(3)
0 件の賞賛
1 解決策
3,201件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Philippe

most probably this is i.MX6 USB port performance limitation (link below),

20-25MB/s according link below (about 1280x720@10 fps),

real limit actually depends on board configuration

https://community.freescale.com/message/353963#353963

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
5 返答(返信)
3,202件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Philippe

most probably this is i.MX6 USB port performance limitation (link below),

20-25MB/s according link below (about 1280x720@10 fps),

real limit actually depends on board configuration

https://community.freescale.com/message/353963#353963

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
1,065件の閲覧回数
kailas_kharse
Contributor IV

Hello @Igor 

I am not able to open the below link.
https://community.freescale.com/message/353963#353963

Can you please help here?

Question:
1. I am using a UVC camera on i.mx6 dual processor, how can I decode MJPEG to stream video upto 1080p 30FPS? 

0 件の賞賛
3,201件の閲覧回数
philippeballeyd
Contributor IV

What do you mean by "real limit actually depends on board configuration"?

Does this mean the problem only appears on the evaluation board?

0 件の賞賛
3,201件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Philippe

I meant software load: with rich GUI performance

will be less. I doubt if 20-25MB/s may be exceeded.

~igor

0 件の賞賛
3,201件の閲覧回数
philippeballeyd
Contributor IV

When i add GST_DEBUG=3 before my gst-launch command, some warning shows up.

The report is in attachment

0 件の賞賛