I configured the gstreamer pipe line as follows.
-->> imxv4l2src device=/dev/video0 ! imv4l2sink
Before Status GST_STATE_PLAYING
g_object_set(src,device"/dev/video1", NULL)
You can select a camera with the command.
but gst_element_set_state(pipeline, GST_STATE_PLAYING);
g_object_set(src,device"/dev/video1", NULL);
command is not executed after the command.
Please tell me how to change the element property to g_object_set.
If src is videootesrc, the g_object_set command changes the property well.
regards.
I'm not sure if I understand it correctly, you play from the video0 firstly, then you want to set pipeline to change to video1? after gst_element_set_state(pipeline, GST_STATE_PLAYING);(this for video0), you want to use "g_object_set(src,device"/dev/video1", NULL);“ to change to video1 from video0, am I right?if yes, maybe you need restart the pipeline, set the PALYING state to NULL firstly, you can refer to the link as below:
"https://stackoverflow.com/questions/37254563/how-to-restart-a-pipeline-when-it-is-in-playing-state"
you also can refer to the source code about setting
"https://github.com/PanderMusubi/gstcam/blob/master/src/gstcam.c"