Hi! Everyone,
Could anyone provide some insights about upgrading gcc 4.4.3 to gcc 4.5.1 in LTIB 2.6.35_1109 and QSB? We need to build some applications but these application can only be compiled under gcc 4.5.1. Thanks!
Vincent
Hi,
The way you have downloaded LTIB from freescale, you have to download the Linaro tool chain.
Check this link https://launchpad.net/gcc-linaro/+milestone/4.5-2012.03
We checked the following link!
https://wiki.linaro.org/Boards/MX53QuickStart
Apparently the steps described in this page do not work. Any other page should we follow?
So, you were talking about adding applications in LTIB and not running applications in linux?
Then you should try the LINARO LTIB. It meets your requirements,
Vincent Chou said:
Should we use steps in the pdf "Adding new toolchain in LTIB" to upgrade the whole toolchain in order to move to gcc 4.5.1? Any potential hazards we may come across?
Yes, the BSP/SDK is free of charge. No royalties of any kind. You can build device drivers and cross compile them easily with the cross-toolchain that comes with the SDK. You don't have to use an IDE. I believe there is no IDE coming with LTIB either.
Is the BSP free of charge? If we use it in a commercial product, do we have to pay certain royalty? If we want to develop certain driver in this BSP, could we use LTIB with this BSP or have to use TimeStorm?
There is one other option. You can register for a free account for i.MX53 on www.timesys.com/register
You will get access to a free BSP/SDK that uses gcc 4.5.3 and the Freescale Linux kernel - 2.6.35 - same as in LTIB, I believe there are 2 BSPs that you can download - small footprint and multimedia.
Don't know about your application API requirements, but you can pick from 1400+ packages (APIs) and build your own, customized version of that BSP/SDK on timesys website as well. HTH
Easy way is to cross compile and port the application binary, if, you are using linux in LTIB.
Would not that be possible?
Using gcc in linux in LTIB, has not been that encouraging for me, when I tried, so I went for CC.