Good afternoon,
I'm following the examples in i.MX_6_G2D_API_User's Guide
My issue is that g2d_blit conversion works, but the returned image is all 0's
All error values for g2d functions are 0, indicating there was no errors
My code is shown below:
If I replace
ExportBmp((uint8_t*)(dst.planes[0]), width, height);
with
ExportBmp((uint8_t*)(src.planes[0]), width, height);
I get the correct image saved,
If I keep it the way it is, I get an image that is all black
My width = 240, height = 180
This API has very little documentation, and it does not mention whether it needs continuous physical memory address, or an array that may be fragmented in memory
I have tried both approaches, and both approaches returned a blank image.
The continuous memory addresses (for the source and destination images) I was able to allocate with ioctl in the IPU
Is there something wrong with the G2D API?
What could be causing this?
Thanks.
void* handle; g2d_open(&handle); src.planes[0] = (int)source; src.left = 0; src.top = 0; src.right = width; src.bottom = height; src.stride = width*2; src.width = width; src.height = height; src.rot = G2D_ROTATION_0; src.format = G2D_RGBA8888; dst.planes[0] = (int)dest; dst.left = 0; dst.top = 0; dst.right = width; dst.bottom = height; dst.stride = width; dst.width = width; dst.height = height; dst.rot = G2D_ROTATION_0; dst.format = G2D_RGBA8888; error =g2d_blit(handle, &src, &dst); error =g2d_finish(handle); error =g2d_close(handle); ExportBmp((uint8_t*)(dst.planes[0]), width, height); | |
已解决! 转到解答。
Resolved:
Using a Continuously allocated buffer was the correct way to do it, however I was passing to the function a virtual pointer created for the application, whereas it required a physical pointer.
I cannot post the full code here, however in order to allocate physical memory in the IPU, you need to:
Do this Twice to obtain a virtualAddr and physAddr for Source and Destination
int* virtualAddr;
int bufferSize = width*height*bytesperpixel;
int physAddr = bufferSize;
int ipuHandle = open("/dev/mxc_ipu", O_RDWR, 0);
ioctl(ipuHandle, IPU_ALLOC, physAddr); //the ioctl function for some reason requires the size of the buffer that it changes to the physical address in memory.
virtualAddr = (int*)mmap(0, bufferSize, PROT_READ | PROT_WRITE, MAP_SHARED, ipuHandle, physAddr);
Then
void* handle;
g2d_open(&handle);
src.planes[0] = physAddrSource;
src.left = 0;
src.top = 0;
src.right = width;
src.bottom = height;
src.stride = width*2;
src.width = width;
src.height = height;
src.rot = G2D_ROTATION_0;
src.format = G2D_RGBA8888;
dst.planes[0] = physAddrDest;
dst.left = 0;
dst.top = 0;
dst.right = width;
dst.bottom = height;
dst.stride = width;
dst.width = width;
dst.height = height;
dst.rot = G2D_ROTATION_0;
dst.format = G2D_RGBA8888;
error =g2d_blit(handle, &src, &dst);
error =g2d_finish(handle);
error =g2d_close(handle);
ExportBmp(virtualAddrDest, width, height);
Resolved:
Using a Continuously allocated buffer was the correct way to do it, however I was passing to the function a virtual pointer created for the application, whereas it required a physical pointer.
I cannot post the full code here, however in order to allocate physical memory in the IPU, you need to:
Do this Twice to obtain a virtualAddr and physAddr for Source and Destination
int* virtualAddr;
int bufferSize = width*height*bytesperpixel;
int physAddr = bufferSize;
int ipuHandle = open("/dev/mxc_ipu", O_RDWR, 0);
ioctl(ipuHandle, IPU_ALLOC, physAddr); //the ioctl function for some reason requires the size of the buffer that it changes to the physical address in memory.
virtualAddr = (int*)mmap(0, bufferSize, PROT_READ | PROT_WRITE, MAP_SHARED, ipuHandle, physAddr);
Then
void* handle;
g2d_open(&handle);
src.planes[0] = physAddrSource;
src.left = 0;
src.top = 0;
src.right = width;
src.bottom = height;
src.stride = width*2;
src.width = width;
src.height = height;
src.rot = G2D_ROTATION_0;
src.format = G2D_RGBA8888;
dst.planes[0] = physAddrDest;
dst.left = 0;
dst.top = 0;
dst.right = width;
dst.bottom = height;
dst.stride = width;
dst.width = width;
dst.height = height;
dst.rot = G2D_ROTATION_0;
dst.format = G2D_RGBA8888;
error =g2d_blit(handle, &src, &dst);
error =g2d_finish(handle);
error =g2d_close(handle);
ExportBmp(virtualAddrDest, width, height);