fsl,legacy-bch-geometry was removed in kernel 5.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fsl,legacy-bch-geometry was removed in kernel 5.4

980 次查看
mohamed-ali_fod
Contributor I

Hello,

The device tree property fsl,legacy-bch-geometry which was available in kernel 4.19 is no more present in kernel 5.4, could you please explain how to handle the legacy bch geometry in this case? because in kernel 5.4 the rootfs cannot be mounted form nand flash due to the following error: ubi0 error: ubi_io_read: error -74 (ECC error) while reading 64 bytes from PEB

Note: fsl,legacy-bch-geometry was the solution to fix ubi_io error in 4.19 kernel, below is the thread for reference:

https://community.nxp.com/t5/i-MX-Processors/IMX6-ubi0-attaching-fail-Kernel-4-19-35-uboot-2014-07/m...

Best Regards,

Mohamed Ali

0 项奖励
回复
2 回复数

969 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

915 次查看
mohamed-ali_fod
Contributor I

Hi Igor,

I am aware about mentioned fix for 4.19 kernel but I am looking for fix of the 5.4 kernel?

Thanks,

Mohamed Ali

0 项奖励
回复