Hi,
Does anyone have the experience using i.mx8 SPI with multiple devices ?
Initially, I was trying to use ECSPI1, but there's only one CS pin supported on ECSPI.
I read i.mx8m nano reference manual and find that flex spi supports multiple devices.
In figure 10-15, there're 2 pairs of CLK & DATA in parallel mode which is not what I need.
Can I use the individual mode to support 4 devices which are sharing one CLK+MISO+MOSI ?
Is my expectation correct ?
Attach the figure10-15 for reference.
Thanks.
解決済! 解決策の投稿を見る。
Hi Luke
>I was trying to use ECSPI1, but there's only one CS pin supported on ECSPI.
one can use gpio as CS as described in linux documentation "- cs-gpios : GPIOs to use as chip selects"
>In figure 10-15, there're 2 pairs of CLK & DATA in parallel mode which is not what I need.
>Can I use the individual mode to support 4 devices which are sharing one CLK+MISO+MOSI ?
>Is my expectation correct ?
not sorry. Only option as described exactly in Figure10-15 is possible.
Best regards
igor
Hi Luke
>I was trying to use ECSPI1, but there's only one CS pin supported on ECSPI.
one can use gpio as CS as described in linux documentation "- cs-gpios : GPIOs to use as chip selects"
>In figure 10-15, there're 2 pairs of CLK & DATA in parallel mode which is not what I need.
>Can I use the individual mode to support 4 devices which are sharing one CLK+MISO+MOSI ?
>Is my expectation correct ?
not sorry. Only option as described exactly in Figure10-15 is possible.
Best regards
igor
Hi Igor,
Thanks for the confirmation!
The good news is that I can discuss further with HW reviewer.