Hi,
I have imx6ul dev board.
I use flashcp to update data file in the mtd flash device. The mtd partition is created through uboot as ubi format. The flashcp doesn't return any errors. After copy, the flash partition causes the problem.
At uboot, the command :
ubi part nand0,6
returns error:
ubi int err 22
which is working before flashcp command
The kernel uses
.compatible = "fsl,imx6ul-gpmi-nand", device driver (gpmi-nand.c)
the gpmi_nand_id_table[] includes imx6ul-gpmi-nand.
What else needs to be set or corrected?
Thank You,
David Zhou
已解决! 转到解答。
Hi David
one can try with latest L4.9.11 nxp official kernel described on
and post issue on kernel mail list, note nxp uses only mfg tools as standard
way for updating images.
Majordomo Lists at VGER.KERNEL.ORG
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David
one can try with latest L4.9.11 nxp official kernel described on
and post issue on kernel mail list, note nxp uses only mfg tools as standard
way for updating images.
Majordomo Lists at VGER.KERNEL.ORG
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------