Hi.
I'm running an image on an i.mx6D (build int Yocto).
The image is running from an emmc (Flash) which is around ~16Gb.
When I try to copy some files to the flash (via SSH) I get following problem:
/home/root/nodeJs/.......: No space left on device
I check the size of the disk with df -h, it there should be space left
Filesystem Size Used Avail Use% Mounted on
/dev/root 15G 9.5G 4.1G 70% /
devtmpfs 342M 4.0K 342M 1% /dev
tmpfs 502M 164K 502M 1% /run
tmpfs 502M 43M 460M 9% /var/volatile
/dev/mmcblk0p1 8.0M 8.0M 24K 100% /media/mmcblk0p1
Is there some setup I need to do to tell it that we are using 16 Gb disk when I compile or maybe some config file under /etc?
Thanks,
Niklas
解決済! 解決策の投稿を見る。
I found the problem.
Seems like I ran out of inodes (df -i, show Ifree = 0).
I had to remove some docker images (seems like there was an issue that inodes where not released after building docker images).
I found the problem.
Seems like I ran out of inodes (df -i, show Ifree = 0).
I had to remove some docker images (seems like there was an issue that inodes where not released after building docker images).
Hello Niklas,
Thanks for sharing your solution with the Community!
Best regards!
/Carlos