Hi,All,
I build mini profile enviroment in custom board. The problem is that I can not login into system. I have try to use rootfs.tar.bz in MFG, it does not work.
But if I use ubuntu demo file system, it works well.
I think the problem is script about rc.conf or rcS,but I don't know how to modify it.If someone can give me a hint,that will be appreciated.
The syslog shows below.
EXT3-fs: barriers not enabled
24bit read error, ret = -5
24bit write error, ret = -5
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p1): using internal journal
EXT3-fs (mmcblk0p1): recovery complete
EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:1.
Freeing init memory: 140K
starting pid 1171, tty '': '/etc/rc.d/rcS'
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Setting the hostname to freescale
Mounting filesystems
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
starting pid 2139, tty '': '-/sbin/getty -L ttymxc0 115200 vt100'
arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4
root filesystem built on Wed, 12 Jun 2013 19:18:43 +0800
Freescale Semiconductor, Inc.
freescale login:
Reagrds,
Haifeng
Hi,Leonardo,
I used rootfs.tar.bz2 built in the MFG.The u-boot.bin and uImage are generated by ltib.
There is no error at the stage of downloading files. I can't login into file system when I input "root" in prompt freescale login:
as the same as I download these files by command dd. If I deselected the []boot up with a tty and login under ltib top menu,
the prompt shows that the currect user is root,but there is response yet if I input command.
I think the error caused by script. How do you think of this question?
Regards,
Haifeng